<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GSM fecility on sabresd board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GSM-fecility-on-sabresd-board/m-p/475998#M75487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sachu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM can be accessed using AT commands, also&lt;/P&gt;&lt;P&gt;3G modem Huawei EM770W is supported in Android&lt;/P&gt;&lt;P&gt;(refer to attached Release Notes p.4):&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/536286"&gt;Re: SIM card Connector port sabresd board reg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Dec 2015 09:26:04 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-15T09:26:04Z</dc:date>
    <item>
      <title>GSM fecility on sabresd board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GSM-fecility-on-sabresd-board/m-p/475997#M75486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai Sir ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have imx6qsabresd&amp;nbsp; evaluation kit with me. I flashed the lolipop android prebuilt image on sabresd board. i found that in board there is one CON1-SIM card connector .&lt;/P&gt;&lt;P&gt;i put one sim on that port&amp;nbsp; if this board have GSM fecility for calling /not? otherwise it only support messaging ? in android OS i found only messaging option .&lt;/P&gt;&lt;P&gt;how can i check this one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 07:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GSM-fecility-on-sabresd-board/m-p/475997#M75486</guid>
      <dc:creator>sachusanal</dc:creator>
      <dc:date>2015-12-10T07:47:10Z</dc:date>
    </item>
    <item>
      <title>Re: GSM fecility on sabresd board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GSM-fecility-on-sabresd-board/m-p/475998#M75487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sachu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM can be accessed using AT commands, also&lt;/P&gt;&lt;P&gt;3G modem Huawei EM770W is supported in Android&lt;/P&gt;&lt;P&gt;(refer to attached Release Notes p.4):&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/536286"&gt;Re: SIM card Connector port sabresd board reg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 09:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GSM-fecility-on-sabresd-board/m-p/475998#M75487</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-15T09:26:04Z</dc:date>
    </item>
  </channel>
</rss>