<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 mirror display in imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475894#M75473</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a mirrored display between the LVDS and HDMI.&amp;nbsp; ldb is mxcfb0 and hdmi is mxcfb1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if i do not add video=mxcfb0:off in bootargs then the ldb shows up and there is nothing on the HDMI. In this case I can test HDMI by dumping some pixels onto the HDMI frame-buffer by using echo command ..like &lt;BR /&gt;&lt;SPAN style="font-family: 'book antiqua', palatino;"&gt;&lt;EM&gt;echo "hello nxp community" &amp;gt; /dev/fb2.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I add video=mxcfb0:off in the command line then the primary display is HDMI and there are no frambuffers for the LDB device.&lt;/P&gt;&lt;P&gt;I have already tried "&lt;A _jive_internal="true" href="https://community.nxp.com/thread/313507"&gt;Can I mirror a LVDS channel on HDMI?&lt;/A&gt; ​" but it did not prove any good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do i need to do something else to support a mirrored display between the two framebuffers ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: ldb is using ipuID=1 displayID=0 ("overlayed") and HDMI is using ipu1 displayID=1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover what do these kernel parameters do "&lt;STRONG&gt;&lt;EM&gt;di0_primary ldb=di1&lt;/EM&gt;&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Jan 2016 12:44:55 GMT</pubDate>
    <dc:creator>adnanali</dc:creator>
    <dc:date>2016-01-30T12:44:55Z</dc:date>
    <item>
      <title>mirror display in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475894#M75473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a mirrored display between the LVDS and HDMI.&amp;nbsp; ldb is mxcfb0 and hdmi is mxcfb1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if i do not add video=mxcfb0:off in bootargs then the ldb shows up and there is nothing on the HDMI. In this case I can test HDMI by dumping some pixels onto the HDMI frame-buffer by using echo command ..like &lt;BR /&gt;&lt;SPAN style="font-family: 'book antiqua', palatino;"&gt;&lt;EM&gt;echo "hello nxp community" &amp;gt; /dev/fb2.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I add video=mxcfb0:off in the command line then the primary display is HDMI and there are no frambuffers for the LDB device.&lt;/P&gt;&lt;P&gt;I have already tried "&lt;A _jive_internal="true" href="https://community.nxp.com/thread/313507"&gt;Can I mirror a LVDS channel on HDMI?&lt;/A&gt; ​" but it did not prove any good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do i need to do something else to support a mirrored display between the two framebuffers ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: ldb is using ipuID=1 displayID=0 ("overlayed") and HDMI is using ipu1 displayID=1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Moreover what do these kernel parameters do "&lt;STRONG&gt;&lt;EM&gt;di0_primary ldb=di1&lt;/EM&gt;&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jan 2016 12:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475894#M75473</guid>
      <dc:creator>adnanali</dc:creator>
      <dc:date>2016-01-30T12:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: mirror display in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475895#M75474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello adnan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It seems that you are using Android system , right ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For android BSP of i.MX6, mxcfb0 must be used. you can't make it off on command line of u-boot.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 06:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475895#M75474</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-02-01T06:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: mirror display in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475896#M75475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nope. I am not using it for android. In the config file&lt;/P&gt;&lt;P&gt;# CONFIG_ANDROID is not set&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 07:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475896#M75475</guid>
      <dc:creator>adnanali</dc:creator>
      <dc:date>2016-02-01T07:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: mirror display in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475897#M75476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using kernel 3.14 if that can help you in figuring out the problem. Found there is a lot of updates in ldb in this kernel version as compared to kernel 3.10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 09:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475897#M75476</guid>
      <dc:creator>adnanali</dc:creator>
      <dc:date>2016-02-02T09:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: mirror display in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475898#M75477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to find a solution to this problem ....kindly bring it to your attention ... Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2016 19:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mirror-display-in-imx6/m-p/475898#M75477</guid>
      <dc:creator>adnanali</dc:creator>
      <dc:date>2016-02-03T19:48:43Z</dc:date>
    </item>
  </channel>
</rss>