<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC13892 : different power source domain  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MC13892-different-power-source-domain/m-p/474222#M75123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MC13892 equivalent to this use method ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;If Yes, Could you tell us the limit in the use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First should be powered up BP, then non-BP power source.&lt;/P&gt;&lt;P&gt;No special requirements for defference value between BP and &lt;/P&gt;&lt;P&gt;non-BP power source.&lt;/P&gt;&lt;P&gt;Input values of SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI &lt;/P&gt;&lt;P&gt;should comply with MC13892 datasheet requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Dec 2015 04:41:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-10T04:41:19Z</dc:date>
    <item>
      <title>MC13892 : different power source domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC13892-different-power-source-domain/m-p/474221#M75122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We consider the MC13892 different power source domains.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In application note AN3867 ( MC13892 Functional Pin Description),&lt;BR /&gt;it says that SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI are connected to BP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But we hope to connect these pins to the another power source other than the BP.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The BP is connected to "A power source".&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI are connected to "B power source".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;Is the MC13892 equivalent to this use method ?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If Yes,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Could you tell us the limit in the use ?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For example, &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; power up sequence related to BP and non-BP power source.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; potential defference value between BP and non-BP power source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, &lt;BR /&gt;Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 02:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC13892-different-power-source-domain/m-p/474221#M75122</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2015-12-10T02:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC13892 : different power source domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC13892-different-power-source-domain/m-p/474222#M75123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MC13892 equivalent to this use method ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;If Yes, Could you tell us the limit in the use ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First should be powered up BP, then non-BP power source.&lt;/P&gt;&lt;P&gt;No special requirements for defference value between BP and &lt;/P&gt;&lt;P&gt;non-BP power source.&lt;/P&gt;&lt;P&gt;Input values of SW1/2/3/4IN and VINUSB2 and VINAUDIO and VINIOHI &lt;/P&gt;&lt;P&gt;should comply with MC13892 datasheet requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 04:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC13892-different-power-source-domain/m-p/474222#M75123</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-10T04:41:19Z</dc:date>
    </item>
  </channel>
</rss>