<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto kernel compilation issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474046#M75072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;have you add one line for your dtb in the makefile?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Mar 2016 03:59:36 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2016-03-15T03:59:36Z</dc:date>
    <item>
      <title>Yocto kernel compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474045#M75071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we used kernel 3.14.28 and yocto .we run below commands &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake linux-imx -c compile -f&lt;/P&gt;&lt;P&gt;its compiled but when we gave build that time only itwill give dtb issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake linux-imx -c build -f&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; scripts/genksyms&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; scripts/kconfig&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; scripts/mod&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; scripts&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; drivers/tty/vt&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CLEAN&amp;nbsp;&amp;nbsp; drivers/video/logo&lt;/P&gt;&lt;P&gt;| make: Leaving directory `/home/vishwa/workspace/veera_checkout_mar10/coderepo1/custom_mar11/tmp/work/imx6_zcam_custom-poky-linux-gnueabi/linux-imx/3.14.28-r0/image/usr/src/kernel'&lt;/P&gt;&lt;P&gt;| NOTE: make -j 4 imx6_zcam_custom.dtb&lt;/P&gt;&lt;P&gt;| make[1]: *** No rule to make target `arch/arm/boot/dts/imx6_zcam_custom.dtb'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| make: *** [imx6_zcam_custom.dtb] Error 2&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (log file is located at /home/vishwa/workspace/veera_checkout_mar10/coderepo1/custom_mar11/tmp/work/imx6_zcam_custom-poky-linux-gnueabi/linux-imx/3.14.28-r0/temp/log.do_install.7621)&lt;/P&gt;&lt;P&gt;ERROR: Task 2 (/home/vishwa/workspace/veera_checkout_mar10/coderepo1/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 407 tasks of which 402 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (407 of 415)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/vishwa/workspace/veera_chec&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 11:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474045#M75071</guid>
      <dc:creator>veeranjaneyulug</dc:creator>
      <dc:date>2016-03-14T11:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto kernel compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474046#M75072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;have you add one line for your dtb in the makefile?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 03:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474046#M75072</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-03-15T03:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto kernel compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474047#M75073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="251177" data-username="veeranjaneyulug" href="https://community.nxp.com/people/veeranjaneyulug"&gt;veeranjaneyulu g&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 'compile' task builds only the zImage while the 'build' task will perform all the tasks for that specific recipe, 'linux-imx' in your case, which includes generating the dtb. So, Your dts is causing this build error. It looks like 'make' is not able to find the dts file&amp;nbsp; "imx6_zcam_custom.dts" in the arch/arm/boot/dts/ directory. Could you confirm that this file is present in the source or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shubham&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 04:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474047#M75073</guid>
      <dc:creator>shubhamsanghvi</dc:creator>
      <dc:date>2016-03-15T04:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto kernel compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474048#M75074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes that imx6_zcam_custom.dts is there in arch/arm/boot/dts directory .And Make file also i added imx6_zcam_custom.dtb line ..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 04:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-kernel-compilation-issue/m-p/474048#M75074</guid>
      <dc:creator>veeranjaneyulug</dc:creator>
      <dc:date>2016-03-15T04:42:48Z</dc:date>
    </item>
  </channel>
</rss>