<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Sata link down in kernel (3.14.28) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472911#M74831</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jifang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if it is detected in uboot, then seems in linux signal is noisy due to&lt;/P&gt;&lt;P&gt;more power consumption: please check ripples on VDDARM_CAP&lt;/P&gt;&lt;P&gt;and VDDSOC_CAP, should be less than 5% &lt;/P&gt;&lt;P&gt;and SATA Phy strength and sensitivity levels, they are defined in&lt;/P&gt;&lt;P&gt;IOMUX GPR13&amp;nbsp; in ../driver/ata/ahci_imx.c&lt;/P&gt;&lt;P&gt;one can set them to values used by uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Apr 2016 01:27:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-04-25T01:27:53Z</dc:date>
    <item>
      <title>Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472910#M74830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sata can't be detected when I tested with kernel 3.10.53 and 3.14.28, but it works in uboot.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My test environment and procedures:&lt;/P&gt;&lt;P&gt;Processor: i.MX6Q&lt;/P&gt;&lt;P&gt;Reference board: &lt;SPAN style="font-size: 10.0pt; font-family: TimesLTStd-Roman;"&gt;imx6qsabresd&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;a) boot with mfg tool using micro usb cable.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot with mfg tool is only for my testing, in production it boots from flash .&lt;/P&gt;&lt;P&gt;b) kernel and rootfs are in SD card.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Test with kernel (linux-2.6-imx-rel_imx_3.10.53_1.1.0_ga.zip) &amp;amp; uboot (rel_imx_3.10.53_1.1.1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sata can be detected in uboot and get manufacture, capacity info, but can't be detected in kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; Prints in dmesg: &lt;/P&gt;&lt;P&gt;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp; Wait for CR ACK error!&lt;/P&gt;&lt;P&gt;&amp;nbsp; sata phy RX_PLL is stable!&lt;/P&gt;&lt;P&gt;&amp;nbsp; ahci: SSS flag set, parallel bus scan disabled&lt;/P&gt;&lt;P&gt;&amp;nbsp; ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst&lt;/P&gt;&lt;P&gt;&amp;nbsp; scsi0 : ahci_platform&lt;/P&gt;&lt;P&gt;&amp;nbsp; ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71&lt;/P&gt;&lt;P&gt;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp; sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;&amp;nbsp; sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;&amp;nbsp; sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;&amp;nbsp; sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode&lt;/P&gt;&lt;P&gt;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp; ata1: SATA link down (SStatus 0 SControl 300)&lt;/P&gt;&lt;P&gt;&amp;nbsp; ata1.00: link offline, clearing class 1 to NONE&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Test with kernel (rel_imx_3.14.28_1.0.0_ga.zip) &amp;amp; uboot (rel_imx_3.14.28_1.0.0_ga)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sata still can be detected in uboot, but can't be detected in kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; And after upraged to kernel 3.14.28, I got one more issue is that i2c0 can't be detected which works fine with 3.10.53.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I attached my linux config, device tree and log which I used with 3.14.28.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is why i2c0 can't be detected any more with the new kernel, i2c0's definition in device tree I didn't change.&lt;/P&gt;&lt;P&gt;I tried several different Sata disks, they are all can be detected in uboot, but not in kernel.&lt;/P&gt;&lt;P&gt;I think there maybe something wrong&amp;nbsp; in linux config or device tree.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll really appreciate if someone can help me sort it out.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336696"&gt;ag13008_linux_defconfig.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336696"&gt;imx6q-ag13008b.dts.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336696"&gt;log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Apr 2016 01:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472910#M74830</guid>
      <dc:creator>fang</dc:creator>
      <dc:date>2016-04-24T01:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472911#M74831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jifang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if it is detected in uboot, then seems in linux signal is noisy due to&lt;/P&gt;&lt;P&gt;more power consumption: please check ripples on VDDARM_CAP&lt;/P&gt;&lt;P&gt;and VDDSOC_CAP, should be less than 5% &lt;/P&gt;&lt;P&gt;and SATA Phy strength and sensitivity levels, they are defined in&lt;/P&gt;&lt;P&gt;IOMUX GPR13&amp;nbsp; in ../driver/ata/ahci_imx.c&lt;/P&gt;&lt;P&gt;one can set them to values used by uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 01:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472911#M74831</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-25T01:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472912#M74832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;I compared SATA parameters in uboot and kernel, found that TXBOOST and TX_LVL is different.&lt;/P&gt;&lt;P&gt;Today is holiday, I'll try it tomorrow.&lt;/P&gt;&lt;P&gt;One more issue is that i2c-0 isn't detected after I upgrade to the new kernel.&lt;/P&gt;&lt;P&gt;Do you know anything conflict in these two version kernels?&lt;/P&gt;&lt;P&gt;I didn't change the i2c-0 definition in device tree.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 04:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472912#M74832</guid>
      <dc:creator>fang</dc:creator>
      <dc:date>2016-04-25T04:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472913#M74833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I set the Sata configuration parameter the same as in the uboot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It still can't be detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# dmesg | grep sata&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.205555] ahci-imx 2200000.sata: fsl,transmit-level-mV value 1104, using 00000044&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.205566] ahci-imx 2200000.sata: fsl,transmit-boost-mdB value 0, using 00000000&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.205575] ahci-imx 2200000.sata: fsl,transmit-atten-16ths value 9, using 00002000&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.205583] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.208407] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.208439] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.208452] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.593187] ahci-imx 2200000.sata: no device found, disabling link.&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.593198] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 03:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472913#M74833</guid>
      <dc:creator>fang</dc:creator>
      <dc:date>2016-04-26T03:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472914#M74834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jifang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had you tried on Sabre board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 04:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472914#M74834</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-26T04:27:08Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472915#M74835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried on our board, it's reference board is imx6qsabresd.&lt;/P&gt;&lt;P&gt;I was told it's nearly the same as the reference board. &lt;/P&gt;&lt;P&gt;I couldn't find &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;VDDARM_CAP in schemetic.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;And I just checked &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;VDDSOC_CAP, &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Without sata inserted, it's value is about 1.2v, and ripple 4%~8%, most of the time is 5%.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;With sata inserted, it's value is about 1.188v, sometimes it jumps to 1.25v (half second).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I'm not hardware engineer, and I don't know it's correct or not.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 04:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472915#M74835</guid>
      <dc:creator>fang</dc:creator>
      <dc:date>2016-04-26T04:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472916#M74836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I fixed i2c-0 issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sata I'm using is SamSung SSD 850 EVO mSata and Intel SSD.&lt;/P&gt;&lt;P&gt;It shares slot with 3G modem, modem works fine in 3.10.53 but failed in 3.14.28.&lt;/P&gt;&lt;P&gt;I created a thread for modem issue.&lt;A href="https://community.nxp.com/thread/391185"&gt;Sierra 3G modem in Linux 3.14.28&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For debug sata, I added three prints in function *ata_dev_next in libata-core.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Uboot3.10.53 + Kernel3.10.53 + prints in libata-core.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sata is detected when warm reset and failed when cold reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Uboot3.14.28 + Kernel3.14.28 +/- prints in libata-core.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sata isn't detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Uboot3.10.53 + Kernel3.14.28 + prints in libata-core.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sata is detected in both warm and cold reset, I tested over 10 times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the test, I think it's a timing issue. &lt;/P&gt;&lt;P&gt;It's failed when I try to add more or less prints, only works with three prints.&lt;/P&gt;&lt;P&gt;I try to figure out a proper place to add some delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know you have rich expericence in imx platform and your service policy.&lt;/P&gt;&lt;P&gt;Any thoughts about the issue is appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 May 2016 00:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472916#M74836</guid>
      <dc:creator>fang</dc:creator>
      <dc:date>2016-05-01T00:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Sata link down in kernel (3.14.28)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472917#M74837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;to test if this is caused by noise&lt;/P&gt;&lt;P&gt;one can try to run minimal image or add capacitors to VDDSOC_CAP&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 00:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sata-link-down-in-kernel-3-14-28/m-p/472917#M74837</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-03T00:57:06Z</dc:date>
    </item>
  </channel>
</rss>