<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx28 fuse programming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471840#M74720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;0x8007001F - A device attached to the system is not functioning.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;Please check if the BitBurner is working on the i.MX28 EVK. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;&amp;nbsp; If it works for the EVK then there is probably something wrong with the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;customer's specific HW configuration. For the BitBurner operations, the i.MX28 &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;must enter recovery mode, which can be seen as a USB human interface device in &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;the windows device manager.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Apr 2016 02:11:28 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-04-27T02:11:28Z</dc:date>
    <item>
      <title>imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471835#M74715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;im currently looking for the "best" way to program the fuse-cells for my custom-board with the imx28. I want to use HAB and encryption feature of the processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have some questions regarding the procedures:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. is it necessary to use usb-recovery modus in general to program the fuses or only if i want to use the mfgtool or the bit-burner?&lt;/P&gt;&lt;P&gt;2. when i get the generated *.sb file with the HAB-related signature fuses, what are the possibilities to set the fuses with this sb file? can i also boot from sd to apply those values?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 16:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471835#M74715</guid>
      <dc:creator>markusvalentin</dc:creator>
      <dc:date>2016-02-18T16:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471836#M74716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Markus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. for fuse burning one can use OBDS (stmp_otp.c)&lt;/P&gt;&lt;P&gt;Lab and Test Software (1)&lt;/P&gt;&lt;P&gt;On-Board Diagnostic Suit for the i.MX28 (REV 1)&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx28-processors/i.mx28-evaluation-kit:MCIMX28EVKJ?fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx28-processors/i.mx28-evaluation-kit:MCIMX28EVKJ?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX28 Evaluation Kit|NXP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;2. one can write own application (using above example) and put it in&lt;/P&gt;&lt;P&gt;*.sb image or sd card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 01:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471836#M74716</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-19T01:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471837#M74717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Please refer to section 6 (Manage the electrical fuses) of the app note &lt;BR /&gt;AN4555 (Secure Boot with i.MX28 HAB Version 4).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4555.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4555.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4555.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 03:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471837#M74717</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-19T03:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471838#M74718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi igor,&lt;/P&gt;&lt;P&gt;yeah&amp;nbsp; the obds seems to be a nice tool. I would like to start it via usb-recovery but i can't get it booting because the *.bd file seems to be not correct, is it generally possible to boot it via usb?&amp;nbsp; do you have a hint for me? &lt;/P&gt;&lt;P&gt;i would love to programm the fuses without windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 10:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471838#M74718</guid>
      <dc:creator>markusvalentin</dc:creator>
      <dc:date>2016-04-26T10:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471839#M74719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i generated a OtpInit.sb file as stated in the AN, when i try to burn the fuses via BitInit (on winxp 32,win8 32). On every platform i get the same error. What is this about? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35573iC3B53B4C09AC0141/image-size/large?v=v2&amp;amp;px=999" title="bit_initr.png" alt="bit_initr.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 10:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471839#M74719</guid>
      <dc:creator>markusvalentin</dc:creator>
      <dc:date>2016-04-26T10:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471840#M74720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;0x8007001F - A device attached to the system is not functioning.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;Please check if the BitBurner is working on the i.MX28 EVK. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;&amp;nbsp; If it works for the EVK then there is probably something wrong with the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;customer's specific HW configuration. For the BitBurner operations, the i.MX28 &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;must enter recovery mode, which can be seen as a USB human interface device in &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;the windows device manager.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 02:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471840#M74720</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-27T02:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471841#M74721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that i am already using the evk and it appears as HID Device. (as you can see in the "german" screenshot). Do you have any other hint? if not i will try to get a "new" processor on my evk.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35874i14C9E86620BF57CB/image-size/large?v=v2&amp;amp;px=999" title="windooze.png" alt="windooze.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 12:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471841#M74721</guid>
      <dc:creator>markusvalentin</dc:creator>
      <dc:date>2016-04-27T12:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 fuse programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471842#M74722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Perhaps it is OS related issue (Win 8, 10, USB3 presence). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 May 2016 08:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-fuse-programming/m-p/471842#M74722</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-05-18T08:14:57Z</dc:date>
    </item>
  </channel>
</rss>