<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can i have example source for EMIF(External memory interface) function? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471574#M74661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6DualLite processor has many various interfaces to receive data from FPGA. Those are the parallel External Memory Interface Module (EIM, primarily meant for connection of an external SRAM/NOR Flash like memories), parallel Camera Sensor Interface (CSI) that allows raw data transfer to memory, PCIe (if supported by FPGA). The particular connection method is FPGA-dependent.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 11:02:01 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-06-15T11:02:01Z</dc:date>
    <item>
      <title>Can i have example source for EMIF(External memory interface) function?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471573#M74660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I check i.mx6dl interface for data transfer from fpga chip.&lt;/P&gt;&lt;P&gt;so.. if i.mx6 sabresd board can use EMIF function, can i have example code or manual?&lt;/P&gt;&lt;P&gt;I already search unit_test example folder but i can not find EMIF file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you know every information about EMIF, reply please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 01:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471573#M74660</guid>
      <dc:creator>hanseunglee</dc:creator>
      <dc:date>2016-06-02T01:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: Can i have example source for EMIF(External memory interface) function?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471574#M74661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6DualLite processor has many various interfaces to receive data from FPGA. Those are the parallel External Memory Interface Module (EIM, primarily meant for connection of an external SRAM/NOR Flash like memories), parallel Camera Sensor Interface (CSI) that allows raw data transfer to memory, PCIe (if supported by FPGA). The particular connection method is FPGA-dependent.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 11:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471574#M74661</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-06-15T11:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can i have example source for EMIF(External memory interface) function?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471575#M74662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hanseung&lt;/P&gt;&lt;P&gt;I am glad to read your article for EIM and FPGA.I am studying them in our work. But&amp;nbsp;I meet a hard problem that the signal is not produced in the EIM bus. I hope you can help me to share your code. sincerely! I look forward to your replay.&lt;/P&gt;&lt;P&gt;Rui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 02:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-have-example-source-for-EMIF-External-memory-interface/m-p/471575#M74662</guid>
      <dc:creator>ruiguo</dc:creator>
      <dc:date>2016-10-31T02:10:36Z</dc:date>
    </item>
  </channel>
</rss>