<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MX233 LCD flicker in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX233-LCD-flicker/m-p/179988#M7466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have attached a 240x320 RGB LCD to MX233. LCDIF is configured to DOTCLK mode, pixel clock is 10Mhz and vsync is 60Hz.&lt;/P&gt;&lt;P&gt;The framebuffer driver is using double frame buffer. It is OK to display a still picture. As a test, the two buffers are initialized in different color. Then, I run a test app which calls ioctl FBIOPAN_DISPLAY to switch between the two buffers and flicker happens.&lt;/P&gt;&lt;P&gt;I have traced the driver, ioctl FBIOPEN_DISAPLY simply updates the register HW_LCDIF_NEXT_BUF. I am not sure if the flicker caused by updating HW_LCDIF_NEXT_BUF or some other reasons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Oct 2011 04:57:17 GMT</pubDate>
    <dc:creator>yfwong1z</dc:creator>
    <dc:date>2011-10-27T04:57:17Z</dc:date>
    <item>
      <title>MX233 LCD flicker</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX233-LCD-flicker/m-p/179988#M7466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have attached a 240x320 RGB LCD to MX233. LCDIF is configured to DOTCLK mode, pixel clock is 10Mhz and vsync is 60Hz.&lt;/P&gt;&lt;P&gt;The framebuffer driver is using double frame buffer. It is OK to display a still picture. As a test, the two buffers are initialized in different color. Then, I run a test app which calls ioctl FBIOPAN_DISPLAY to switch between the two buffers and flicker happens.&lt;/P&gt;&lt;P&gt;I have traced the driver, ioctl FBIOPEN_DISAPLY simply updates the register HW_LCDIF_NEXT_BUF. I am not sure if the flicker caused by updating HW_LCDIF_NEXT_BUF or some other reasons.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2011 04:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX233-LCD-flicker/m-p/179988#M7466</guid>
      <dc:creator>yfwong1z</dc:creator>
      <dc:date>2011-10-27T04:57:17Z</dc:date>
    </item>
  </channel>
</rss>