<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Secure boot for i.mx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470574#M74462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; There is no special descriptions how to load and flash images from SD.&lt;BR /&gt;But it is enough to look over&amp;nbsp; "ucl2.xml" file of MFG in order to understand main&lt;/P&gt;&lt;P&gt;Linux commands and procedures, used to deploy the image. The MFG &lt;BR /&gt;is used just to load minimal Linux via USB. You may use the same sequence,&lt;/P&gt;&lt;P&gt;assuming all the needed image files are located in Linux file system, which &lt;/P&gt;&lt;P&gt;in itself boots from SD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Feb 2016 07:05:53 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-02-22T07:05:53Z</dc:date>
    <item>
      <title>Secure boot for i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470573#M74461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After getting the uboot-singed-pad.bin , how should we flash it via SD? If you have a separate process for flashing this uboot-singed-pad.bin, provide us the process to flash it. If we go by the process of burning eMMC by Mfg tool it takes only .imx and .img for u-boot and kernal. But as per the HAB process document we&amp;nbsp; can authenticate only u-boot.bin files.Is there any separate method other than using Mfg tool to flash the binary images that are authenticated by HAB?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 11:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470573#M74461</guid>
      <dc:creator>aishashaik</dc:creator>
      <dc:date>2016-02-19T11:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot for i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470574#M74462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; There is no special descriptions how to load and flash images from SD.&lt;BR /&gt;But it is enough to look over&amp;nbsp; "ucl2.xml" file of MFG in order to understand main&lt;/P&gt;&lt;P&gt;Linux commands and procedures, used to deploy the image. The MFG &lt;BR /&gt;is used just to load minimal Linux via USB. You may use the same sequence,&lt;/P&gt;&lt;P&gt;assuming all the needed image files are located in Linux file system, which &lt;/P&gt;&lt;P&gt;in itself boots from SD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 07:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470574#M74462</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-22T07:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot for i.mx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470575#M74463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 05:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-boot-for-i-mx6/m-p/470575#M74463</guid>
      <dc:creator>aishashaik</dc:creator>
      <dc:date>2016-02-25T05:05:59Z</dc:date>
    </item>
  </channel>
</rss>