<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to use Parallel CSI interface on IMX6Q without decoder in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-Parallel-CSI-interface-on-IMX6Q-without-decoder/m-p/470524#M74452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to interface IMX6Q with a device(an FPGA actually) which directly gives 8 bit YCbCr format output with HSYNC , VSYNC and PIXCLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went through the .dtsi files, the camera driver has been written as a part of the I2C driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, as I am not using any decoder, I need some guidance on&lt;/P&gt;&lt;P&gt;which driver I should use, to capture the CSI data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you your time,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 May 2016 10:55:41 GMT</pubDate>
    <dc:creator>nishad_kamdar</dc:creator>
    <dc:date>2016-05-13T10:55:41Z</dc:date>
    <item>
      <title>How to use Parallel CSI interface on IMX6Q without decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-Parallel-CSI-interface-on-IMX6Q-without-decoder/m-p/470524#M74452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to interface IMX6Q with a device(an FPGA actually) which directly gives 8 bit YCbCr format output with HSYNC , VSYNC and PIXCLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went through the .dtsi files, the camera driver has been written as a part of the I2C driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, as I am not using any decoder, I need some guidance on&lt;/P&gt;&lt;P&gt;which driver I should use, to capture the CSI data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you your time,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 May 2016 10:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-Parallel-CSI-interface-on-IMX6Q-without-decoder/m-p/470524#M74452</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2016-05-13T10:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to use Parallel CSI interface on IMX6Q without decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-Parallel-CSI-interface-on-IMX6Q-without-decoder/m-p/470525#M74453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nishad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems one can try to remove i2c references or write new driver using&lt;/P&gt;&lt;P&gt;guidelines in attached Porting Guide Chapter 7 Supporting the i.MX 6Dual/6Quad/&lt;/P&gt;&lt;P&gt;6Solo/6DualLite Camera Sensor with CSI. As help is attached baremetal sensor&lt;/P&gt;&lt;P&gt;example from sdk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 May 2016 00:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-Parallel-CSI-interface-on-IMX6Q-without-decoder/m-p/470525#M74453</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-14T00:24:38Z</dc:date>
    </item>
  </channel>
</rss>