<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android to use Second Screen</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470466#M74443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reviewing the code in hardware/imx/mx6/hwcomposer/hwc_display.cpp (hwc_judge_display_state), it seems possible to change the initial for loop to start at a higher number.&amp;nbsp;&amp;nbsp; This would populate the struct ctx-&amp;gt;mDispInfo with the higher FB Info.&amp;nbsp;&amp;nbsp; I believe this is similar to the method used in the mx7...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the information in mDispInfo not used by the remainder of the FSL HAL??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jun 2016 21:00:20 GMT</pubDate>
    <dc:creator>mike_sims</dc:creator>
    <dc:date>2016-06-03T21:00:20Z</dc:date>
    <item>
      <title>Android to use Second Screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470464#M74441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a i.mx6 SABRE SD board which has 2 display outputs.&amp;nbsp;&amp;nbsp; I have a fixed function for FB0/FB1 and would like to have Android use the second display at FB2/FB3 instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been pouring through documentation on the web and source code (Android 6.0.1), but it has not become obvious to me how I define which devices are available to Android.&amp;nbsp;&amp;nbsp; I looked in the device specific files of Devices/FSL and Hardware/IMX/mx6 and believe there may be a way to hard-code this in these files, but to date, I have not seen how to configure this at runtime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please point me to how I might accomplish this...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 18:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470464#M74441</guid>
      <dc:creator>mike_sims</dc:creator>
      <dc:date>2016-06-01T18:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: Android to use Second Screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470465#M74442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Even there is a way to modify the source of FB devices,&amp;nbsp; I strongly suggest that you do not do it, because there are drivers in the i.MX like&amp;nbsp; GPU/ VPU&amp;nbsp; that expect to have FB0 and FB1 as the default sources for the LCD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 15:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470465#M74442</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2016-06-03T15:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: Android to use Second Screen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470466#M74443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reviewing the code in hardware/imx/mx6/hwcomposer/hwc_display.cpp (hwc_judge_display_state), it seems possible to change the initial for loop to start at a higher number.&amp;nbsp;&amp;nbsp; This would populate the struct ctx-&amp;gt;mDispInfo with the higher FB Info.&amp;nbsp;&amp;nbsp; I believe this is similar to the method used in the mx7...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the information in mDispInfo not used by the remainder of the FSL HAL??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 21:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-to-use-Second-Screen/m-p/470466#M74443</guid>
      <dc:creator>mike_sims</dc:creator>
      <dc:date>2016-06-03T21:00:20Z</dc:date>
    </item>
  </channel>
</rss>