<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reducing imx6 yocto build size for custom board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-imx6-yocto-build-size-for-custom-board/m-p/470335#M74414</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing special regarding to i.MX. I can provide you some common recomendations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can remove all unnessesary options and modules from the kernel.&lt;/P&gt;&lt;P&gt;For example if you do not need ethernet you can compile the kernel without its support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you need to remove all unnessesary packages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jun 2016 05:55:25 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-06-02T05:55:25Z</dc:date>
    <item>
      <title>Reducing imx6 yocto build size for custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-imx6-yocto-build-size-for-custom-board/m-p/470334#M74413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yocto Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read documents but couldn't find a neat way to reduce the size of sdcard image for the dual-lite SABRE board I have. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our custom board is targeted for 16MB nor flash which uses imx6solo processor. I am using yocto environment and building images using "core-image-base" and "core-image-minimal" that ends up with 100MB/29MB on L4.1.15.x release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand my sdcard image contains uboot+kernel+dts+rootfs. My understanding is uboot+kernel+dts is small &amp;lt;10MB but the file-system is taking more space ( I even tried playing around packages_ipk and packages_rpm with no luck).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please advise?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Swapna &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 14:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-imx6-yocto-build-size-for-custom-board/m-p/470334#M74413</guid>
      <dc:creator>sayi</dc:creator>
      <dc:date>2016-06-01T14:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing imx6 yocto build size for custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-imx6-yocto-build-size-for-custom-board/m-p/470335#M74414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing special regarding to i.MX. I can provide you some common recomendations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can remove all unnessesary options and modules from the kernel.&lt;/P&gt;&lt;P&gt;For example if you do not need ethernet you can compile the kernel without its support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you need to remove all unnessesary packages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 05:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-imx6-yocto-build-size-for-custom-board/m-p/470335#M74414</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-06-02T05:55:25Z</dc:date>
    </item>
  </channel>
</rss>