<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI port via the Audio Code header in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179764#M7429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have developed iMX25 PDK 3stack SPI driver for Nucleus Plus RTOS and tested it with the&amp;nbsp;pin outs&amp;nbsp;available at audio. jac.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Oct 2011 11:02:17 GMT</pubDate>
    <dc:creator>ZaheerAhmad</dc:creator>
    <dc:date>2011-10-25T11:02:17Z</dc:date>
    <item>
      <title>SPI port via the Audio Code header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179763#M7428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone ever tried to run a SPI device off the Audio Code Header on the iMX 25 PDK Personality board?&amp;nbsp; I have a chip with an SPI interface, but it has a few quirks.&amp;nbsp; I need to experiment with the chip first to decide if "so broke" we have to bit-bang it or if the SPI interface on the chip is functional enough to run over SPI.&amp;nbsp; That seems like the easiest access point to an SPI port, but curious if anyone else has tried it.&amp;nbsp; Or if there is a better solution I'm not seeing ....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Oct 2011 21:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179763#M7428</guid>
      <dc:creator>Don_ng</dc:creator>
      <dc:date>2011-10-24T21:44:44Z</dc:date>
    </item>
    <item>
      <title>Re: SPI port via the Audio Code header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179764#M7429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have developed iMX25 PDK 3stack SPI driver for Nucleus Plus RTOS and tested it with the&amp;nbsp;pin outs&amp;nbsp;available at audio. jac.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2011 11:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179764#M7429</guid>
      <dc:creator>ZaheerAhmad</dc:creator>
      <dc:date>2011-10-25T11:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: SPI port via the Audio Code header</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179765#M7430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;i'm working with nucleus ready start on the spi ,actualy i'am trying to make something&amp;nbsp; work with the lwspi driver ,but the problem is that i don't really know how to start ,and the nucleus approach is new to me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Dec 2012 00:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-port-via-the-Audio-Code-header/m-p/179765#M7430</guid>
      <dc:creator>hosnihosni</dc:creator>
      <dc:date>2012-12-15T00:52:58Z</dc:date>
    </item>
  </channel>
</rss>