<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic rgmii loopback test for imx6q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/rgmii-loopback-test-for-imx6q/m-p/468963#M74085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.xm6q based custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are facing packet loss for size 1k+ consistently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To debug the issue &amp;amp; verify the driver, I want to enable the loopback as mention in following.&lt;/P&gt;&lt;P&gt;Receive Control Register (ENET_RCR)[LOOP] = 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this bit is explained as MII internal loopback, To enable loopback we have to set MII_MODE set to 1 &amp;amp; RMII_MODE set to 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could we use this loopback to test the RGMII driver also?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not how to test the loopback for RGMII?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Praveen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Dec 2015 15:29:35 GMT</pubDate>
    <dc:creator>pravverma</dc:creator>
    <dc:date>2015-12-08T15:29:35Z</dc:date>
    <item>
      <title>rgmii loopback test for imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/rgmii-loopback-test-for-imx6q/m-p/468963#M74085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.xm6q based custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are facing packet loss for size 1k+ consistently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To debug the issue &amp;amp; verify the driver, I want to enable the loopback as mention in following.&lt;/P&gt;&lt;P&gt;Receive Control Register (ENET_RCR)[LOOP] = 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this bit is explained as MII internal loopback, To enable loopback we have to set MII_MODE set to 1 &amp;amp; RMII_MODE set to 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could we use this loopback to test the RGMII driver also?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not how to test the loopback for RGMII?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Praveen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 15:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/rgmii-loopback-test-for-imx6q/m-p/468963#M74085</guid>
      <dc:creator>pravverma</dc:creator>
      <dc:date>2015-12-08T15:29:35Z</dc:date>
    </item>
    <item>
      <title>Re: rgmii loopback test for imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/rgmii-loopback-test-for-imx6q/m-p/468964#M74086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Internal MII loopback described in this register supposes only MII not RGMII.&lt;/P&gt;&lt;P&gt;I mean we have only MII loopback in i.MX6Q processor.&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 06:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/rgmii-loopback-test-for-imx6q/m-p/468964#M74086</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-12-11T06:08:30Z</dc:date>
    </item>
  </channel>
</rss>