<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLooking for a HDMI input solution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-HDMI-input-solution/m-p/468751#M74046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am looking for a HDMI input solution for imx6.&lt;/P&gt;&lt;P&gt;Can I get some information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 10:01:41 GMT</pubDate>
    <dc:creator>hyonlim</dc:creator>
    <dc:date>2016-02-18T10:01:41Z</dc:date>
    <item>
      <title>Looking for a HDMI input solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-HDMI-input-solution/m-p/468751#M74046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am looking for a HDMI input solution for imx6.&lt;/P&gt;&lt;P&gt;Can I get some information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 10:01:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-HDMI-input-solution/m-p/468751#M74046</guid>
      <dc:creator>hyonlim</dc:creator>
      <dc:date>2016-02-18T10:01:41Z</dc:date>
    </item>
    <item>
      <title>Re: Looking for a HDMI input solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-HDMI-input-solution/m-p/468752#M74047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;None of the i.MX6 series processors has an on-chip HDMI input, so, anyway, an external HDMI receiver/deserializer IC should be used. The example is the following part (please note that this is for reference only, NXP cannot recommend one part vendor over another):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.analog.com/en/products/audio-video/analoghdmidvi-interfaces/analog-hdmidvi-display-interfaces/adv7612.html" rel="nofollow"&gt;http://www.analog.com/en/products/audio-video/analoghdmidvi-interfaces/analog-hdmidvi-display-interfaces/adv7612.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It then can be connected to the processor's Camera Sensor Input (CSI) parallel port as a regular video capture device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another possible solution is the HDMI to MIPI CSI-2 bridge, such as the following ones:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://toshiba.semicon-storage.com/us/product/assp/interface-bridge/hdmi.html" rel="nofollow"&gt;http://toshiba.semicon-storage.com/us/product/assp/interface-bridge/hdmi.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.auvidea.eu/index.php/theme-styles/2014-12-30-22-32-06/b102" rel="nofollow"&gt;http://www.auvidea.eu/index.php/theme-styles/2014-12-30-22-32-06/b102&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 11:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Looking-for-a-HDMI-input-solution/m-p/468752#M74047</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-02-18T11:30:48Z</dc:date>
    </item>
  </channel>
</rss>