<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unexpected UART_RTS_B interrupt on i.MX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468673#M74015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear gusarambula-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;We still have this problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry, We use UART6. However, We do not use RTS and CTS function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, the RTSDEN bit of the UART6_UCR1 register is set in "1: RTS Delta Interrupt Enable".&lt;/P&gt;&lt;P&gt;In Linux BSP "drivers/tty/serial/imx.c" , this is set by default. (We do not make any modifications.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the explanation of RTSDEN bit, "The current status of the RTS_B pin is read in the RTSS bit."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the register setting related to the RTS_B pin is as follows,&lt;/P&gt;&lt;P&gt;Is a status of CSI_VSYNC pin read as a RTS_B status ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Register setting related to the RTS_B pin&amp;gt;&lt;/P&gt;&lt;P&gt;- The IOMUXC_UART6_RTS_B_SELECT_INPUT register is a default state, too&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 00:CSI_VSYNC_ALT8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- And, the IOMUXC_SW_MUX_CTL_PAD_CSI_VSYNC register is set in ALT1:USDHC_CLK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The CSI_VSYNC pad is assigned to USDHC_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55790iE0B8D9D12B28436D/image-size/large?v=v2&amp;amp;px=999" title="UART6_RTS_B.png" alt="UART6_RTS_B.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to avoid unexpected UART_RTS_B interrupt, should RTSDEN bit be set to Disable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May I have advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Mar 2016 06:55:38 GMT</pubDate>
    <dc:creator>yuuki</dc:creator>
    <dc:date>2016-03-02T06:55:38Z</dc:date>
    <item>
      <title>Unexpected UART_RTS_B interrupt on i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468671#M74013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a problem that RTS_B interrupt occurs though UART6 is not used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU is i.MX6UL.&lt;/P&gt;&lt;P&gt;BSP is L3.14.52_1.1.0-ga&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In IOMUX, the UART6_RTS_B signal is assigned to CSI_VSYNC pin(ALT8) and ENET1_TX_EN pin(ALT1).&lt;/P&gt;&lt;P&gt;However, CSI_VSYNC pin is used as ALT1:USDHC2_CLK and ENET_TX_EN pin is used as ALT0:ENET_TX_EN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Register Seting&amp;gt;&lt;/P&gt;&lt;P&gt; - IOMUXC_SW_MUX_CTL_PAD_ENET1_TX_EN 0x020E00D8&amp;nbsp; 0x00000000&lt;/P&gt;&lt;P&gt; - IOMUXC_SW_MUX_CTL_PAD_CSI_VSYNC&amp;nbsp;&amp;nbsp; 0x020E01DC&amp;nbsp; 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a clock is input into CSI_VSINC pin, an interrupt of UART_RTS_B occurs.&lt;/P&gt;&lt;P&gt;It seems that a signal from CSI_VSYNC pin is entered in RTS of UART port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IOMUXC_UART6_RTS_B_SELECT_INPUT register remains a default value&lt;/P&gt;&lt;P&gt;(0x00000000 :CSI_VSYNC_ALT8 =&amp;gt; UART6_RTS_B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you tell me the method to disable RTS_B interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 14:12:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468671#M74013</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2016-02-18T14:12:27Z</dc:date>
    </item>
    <item>
      <title>Re: Unexpected UART_RTS_B interrupt on i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468672#M74014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuuki,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still having this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend looking for more instances on the Device Tree where there could be a conflict on the function of the pin. Especially make sure that the UART module status is set to disable since it won’t be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 21:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468672#M74014</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-02-25T21:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: Unexpected UART_RTS_B interrupt on i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468673#M74015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear gusarambula-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;We still have this problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry, We use UART6. However, We do not use RTS and CTS function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, the RTSDEN bit of the UART6_UCR1 register is set in "1: RTS Delta Interrupt Enable".&lt;/P&gt;&lt;P&gt;In Linux BSP "drivers/tty/serial/imx.c" , this is set by default. (We do not make any modifications.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the explanation of RTSDEN bit, "The current status of the RTS_B pin is read in the RTSS bit."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the register setting related to the RTS_B pin is as follows,&lt;/P&gt;&lt;P&gt;Is a status of CSI_VSYNC pin read as a RTS_B status ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Register setting related to the RTS_B pin&amp;gt;&lt;/P&gt;&lt;P&gt;- The IOMUXC_UART6_RTS_B_SELECT_INPUT register is a default state, too&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 00:CSI_VSYNC_ALT8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- And, the IOMUXC_SW_MUX_CTL_PAD_CSI_VSYNC register is set in ALT1:USDHC_CLK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The CSI_VSYNC pad is assigned to USDHC_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55790iE0B8D9D12B28436D/image-size/large?v=v2&amp;amp;px=999" title="UART6_RTS_B.png" alt="UART6_RTS_B.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to avoid unexpected UART_RTS_B interrupt, should RTSDEN bit be set to Disable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May I have advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 06:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468673#M74015</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2016-03-02T06:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: Unexpected UART_RTS_B interrupt on i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468674#M74016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuuki,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologized for the delay. Internal architecture do require you to disable the RTSDEN bit in order to avoid an interrupt input on this pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 18:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unexpected-UART-RTS-B-interrupt-on-i-MX6UL/m-p/468674#M74016</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-03-15T18:32:33Z</dc:date>
    </item>
  </channel>
</rss>