<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6 CAN Transceiver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467394#M73766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have designed a custom SoM using the i.MX6Q and have been working with the CAN interface.&amp;nbsp; Following the Sabre AI board we used a 3.3v transceiver so there was no need for level translation between the processor and transceiver.&amp;nbsp; We have run into problems in that the signals coming from the i.MX6Q are not what would be expected.&amp;nbsp; Both the CAN_RX and CAN_TX signals are being driven when sending data.&amp;nbsp; I connected a scope to the CAN_TX and CAN_RX signals without the transceiver being connected and observed the following;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35227iE392F18CF73ABBC2/image-size/large?v=v2&amp;amp;px=999" title="CAN_Signals.jpg" alt="CAN_Signals.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These signals look exactly like what I would expect to see after the transceiver and not coming directly from the i.MX6.&amp;nbsp; I tried connecting these lines directly to another board without using the transceiver and was able to transmit and receive without issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like for someone to shed some light on exactly what is happening here as I can find no mention in the reference design or reference manual that alludes to what could possibly be going on.&amp;nbsp; Is the transceiver built into the SoC and just not mentioned anywhere or do I have the FlexCAN configured in some weird way and it just happens to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jake&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Apr 2016 18:54:15 GMT</pubDate>
    <dc:creator>jakepollex</dc:creator>
    <dc:date>2016-04-21T18:54:15Z</dc:date>
    <item>
      <title>IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467394#M73766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have designed a custom SoM using the i.MX6Q and have been working with the CAN interface.&amp;nbsp; Following the Sabre AI board we used a 3.3v transceiver so there was no need for level translation between the processor and transceiver.&amp;nbsp; We have run into problems in that the signals coming from the i.MX6Q are not what would be expected.&amp;nbsp; Both the CAN_RX and CAN_TX signals are being driven when sending data.&amp;nbsp; I connected a scope to the CAN_TX and CAN_RX signals without the transceiver being connected and observed the following;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35227iE392F18CF73ABBC2/image-size/large?v=v2&amp;amp;px=999" title="CAN_Signals.jpg" alt="CAN_Signals.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These signals look exactly like what I would expect to see after the transceiver and not coming directly from the i.MX6.&amp;nbsp; I tried connecting these lines directly to another board without using the transceiver and was able to transmit and receive without issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like for someone to shed some light on exactly what is happening here as I can find no mention in the reference design or reference manual that alludes to what could possibly be going on.&amp;nbsp; Is the transceiver built into the SoC and just not mentioned anywhere or do I have the FlexCAN configured in some weird way and it just happens to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jake&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 18:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467394#M73766</guid>
      <dc:creator>jakepollex</dc:creator>
      <dc:date>2016-04-21T18:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467395#M73767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jake&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TJA1041AT datasheet used in Sabre AI board&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocuments%2Fdata_sheet%2FTJA1041A.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/documents/data_sheet/TJA1041A.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;on Figure 9 Timing Diagram shows signals from&amp;nbsp; transceiver (CANH and CANL)&lt;/P&gt;&lt;P&gt;and from processor (CAN_RXD, CAN_TXD)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocuments%2Fdata_sheet%2FTJA1041A.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/documents/data_sheet/TJA1041A.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The transceiver receiver will convert the differential analog bus signal on pins CANH &lt;/P&gt;&lt;P&gt;and CANL into processor CAN_RXD digital data,&amp;nbsp; The transceiver transmitter will &lt;/P&gt;&lt;P&gt;convert processor digital data&amp;nbsp; from CAN_TXD&amp;nbsp; into&amp;nbsp; bus CANH and CANL bus&lt;/P&gt;&lt;P&gt;differential analog signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 00:42:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467395#M73767</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-22T00:42:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467396#M73768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick response.&amp;nbsp; The scope shot that I posted is WITH NO CAN TRANSCEIVER CONNECTED.&amp;nbsp; Therefore nothing should be driving the CAN_RX signal.&amp;nbsp; There was nothing connected to the CAN lines when I took the scope shot.&amp;nbsp; How and why is the CAN_RX signal being driven.&amp;nbsp; It is clearly inverted from the CAN_TX signal and not at all what should be present on the CAN_RX even if the transceiver was connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jake&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 15:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467396#M73768</guid>
      <dc:creator>jakepollex</dc:creator>
      <dc:date>2016-04-22T15:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467397#M73769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what are amplitudes for both channels, it is not clear from picture?&lt;/P&gt;&lt;P&gt;Also could you attach pull-down 10Kohm to CAN_RX.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 15:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467397#M73769</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-22T15:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467398#M73770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a rough drawing of the signals I am seeing coming directly from the i.MX6 with NO transceiver connected.&amp;nbsp; The drawing is only to show the voltage levels.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34507i1CCEE6B486235135/image-size/large?v=v2&amp;amp;px=999" title="CAN_Signals_2.JPG" alt="CAN_Signals_2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 17:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467398#M73770</guid>
      <dc:creator>jakepollex</dc:creator>
      <dc:date>2016-04-22T17:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 CAN Transceiver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467399#M73771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;seems smth wrong in schematic or measuring, because&lt;/P&gt;&lt;P&gt;these signals should comply with Table in&lt;/P&gt;&lt;P&gt;sect.4.6.2 General Purpose I/O (GPIO) DC Parameters&lt;/P&gt;&lt;P&gt;i.MX6DQ Datasheet&amp;nbsp; [OVDD is power domain]&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Had you tried to attach pull-down 10Kohm to CAN_RX and test?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Apr 2016 00:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-CAN-Transceiver/m-p/467399#M73771</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-23T00:34:12Z</dc:date>
    </item>
  </channel>
</rss>