<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Enable CSU in imx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466616#M73561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;As per CSU_CSL registers default value ,it has secure read /write permission by default .(CSU_CSL=0x00330033)&lt;/P&gt;&lt;P&gt;I am not getting that even though it has secure read/write access permission then how that peripheral can be accessed from linux kernel.&lt;/P&gt;&lt;P&gt;is it that linux kernel is operating in secure mode?&lt;/P&gt;&lt;P&gt;i want to add CSU for secure and non secure access of peripherals .&lt;/P&gt;&lt;P&gt;so help me on how to enable CSU in imx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Apr 2016 08:41:02 GMT</pubDate>
    <dc:creator>kajalsabhani</dc:creator>
    <dc:date>2016-04-21T08:41:02Z</dc:date>
    <item>
      <title>Enable CSU in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466616#M73561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;As per CSU_CSL registers default value ,it has secure read /write permission by default .(CSU_CSL=0x00330033)&lt;/P&gt;&lt;P&gt;I am not getting that even though it has secure read/write access permission then how that peripheral can be accessed from linux kernel.&lt;/P&gt;&lt;P&gt;is it that linux kernel is operating in secure mode?&lt;/P&gt;&lt;P&gt;i want to add CSU for secure and non secure access of peripherals .&lt;/P&gt;&lt;P&gt;so help me on how to enable CSU in imx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 08:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466616#M73561</guid>
      <dc:creator>kajalsabhani</dc:creator>
      <dc:date>2016-04-21T08:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: Enable CSU in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466617#M73562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. is it that linux kernel is operating in secure mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. The Linux kernel code is executed in the ARM hardware Supervisor mode, so, it has the Secure level of access.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. i want to add CSU for secure and non secure access of peripherals . so help me on how to enable CSU in imx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Please refer to the Chapter 3 of the i.MX6 Series Security Reference Manual document, available for download on the NXP web site (check the "Reference Manuals" section):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Fi.mx-applications-processors%2Fi.mx-6-processors%2Fi.mx6qp%2Fi.mx-6quad-processors-high-performance-3d-graphics-hd-video-arm-cortex-a9-core%3Ai.MX6Q%3Ffpsp%3D1%26tab%3DDocumentation_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6quad-processors-high-performance-3d-graphics-hd-video-arm-cortex-a9-core:i.MX6Q?fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 06:23:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466617#M73562</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-22T06:23:53Z</dc:date>
    </item>
    <item>
      <title>Re: Enable CSU in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466618#M73563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As linux is in supervisor mode and has secured level of access then how i configure linux for user mode and non secure access&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 06:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466618#M73563</guid>
      <dc:creator>kajalsabhani</dc:creator>
      <dc:date>2016-04-22T06:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: Enable CSU in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466619#M73564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not possible to make the Linux kernel run in User mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 07:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466619#M73564</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-22T07:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Enable CSU in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466620#M73565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok .&lt;/P&gt;&lt;P&gt;so using CSU we can provide non secure accesss .&lt;/P&gt;&lt;P&gt;for that SMC (secure monitor calling) is required . right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 07:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enable-CSU-in-imx6/m-p/466620#M73565</guid>
      <dc:creator>kajalsabhani</dc:creator>
      <dc:date>2016-04-22T07:49:23Z</dc:date>
    </item>
  </channel>
</rss>