<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VNC server with frame buffer distribution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VNC-server-with-frame-buffer-distribution/m-p/466284#M73476</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;Until now I have been working with X11 distros and using x11vnc without any problem. I would like to test a FB distro and I would like to know which is the suitable vnc server to add to the distribution and how should I add it (the package name to add to IMAGE_INSTALL).&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;alvaro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 07:13:44 GMT</pubDate>
    <dc:creator>almarto</dc:creator>
    <dc:date>2016-05-12T07:13:44Z</dc:date>
    <item>
      <title>VNC server with frame buffer distribution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VNC-server-with-frame-buffer-distribution/m-p/466284#M73476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;Until now I have been working with X11 distros and using x11vnc without any problem. I would like to test a FB distro and I would like to know which is the suitable vnc server to add to the distribution and how should I add it (the package name to add to IMAGE_INSTALL).&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;alvaro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 07:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VNC-server-with-frame-buffer-distribution/m-p/466284#M73476</guid>
      <dc:creator>almarto</dc:creator>
      <dc:date>2016-05-12T07:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: VNC server with frame buffer distribution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VNC-server-with-frame-buffer-distribution/m-p/466285#M73477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can run VNC server with the command like this on your board:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# /usr/bin/x11vnc -display :0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then you will see such lines among the diasnostics:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VNC desktop is:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx6qdlsolo:0&lt;/P&gt;&lt;P&gt;PORT=5900&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These lines mean that it is #0 X sevrer on the host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And then you can use any of VNC clients to access your VNC server.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=https%3A%2F%2Fhelp.ubuntu.com%2Fcommunity%2FVNC%2FClients" rel="nofollow" target="_blank"&gt;https://help.ubuntu.com/community/VNC/Clients&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 May 2016 04:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VNC-server-with-frame-buffer-distribution/m-p/466285#M73477</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-05-24T04:13:57Z</dc:date>
    </item>
  </channel>
</rss>