<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMPF0100 POWERON in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-POWERON/m-p/466183#M73455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Sabre board for Smart Devices of iMX6, the PMIC power on pin is connected to VSNVS rail and this confuses me. If PWRON pin is configured as level sensitive such that active high turns the device on, how can it turn itself on when is is not yet turned on and there is no voltage on the VSNVS output? Can someone explain? Perhaps I am misinterpreting the situation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 12:56:51 GMT</pubDate>
    <dc:creator>atillametetured</dc:creator>
    <dc:date>2016-03-31T12:56:51Z</dc:date>
    <item>
      <title>MMPF0100 POWERON</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-POWERON/m-p/466183#M73455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the Sabre board for Smart Devices of iMX6, the PMIC power on pin is connected to VSNVS rail and this confuses me. If PWRON pin is configured as level sensitive such that active high turns the device on, how can it turn itself on when is is not yet turned on and there is no voltage on the VSNVS output? Can someone explain? Perhaps I am misinterpreting the situation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 12:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-POWERON/m-p/466183#M73455</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-03-31T12:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100 POWERON</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-POWERON/m-p/466184#M73456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt; The PMIC VSNVS pin is connected to Li-cel, assuming it is always ON power,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;or it is powered first during PMIC Start-up Sequence. Please refer to PMIC&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="a______"&gt;&lt;SPAN class="tm7"&gt;Datasheet about its power up sequence.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Apr 2016 02:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-POWERON/m-p/466184#M73456</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-01T02:29:45Z</dc:date>
    </item>
  </channel>
</rss>