<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6Q DDR3 clock problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466178#M73452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;generated script just calculates MMC/DDR settings but does not set CCM frequencies.&lt;/P&gt;&lt;P&gt;This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.&lt;/P&gt;&lt;P&gt;So there are no indication of any&amp;nbsp; issues with your i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Dec 2015 06:02:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-08T06:02:40Z</dc:date>
    <item>
      <title>i.MX6Q DDR3 clock problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466177#M73451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For troubleshooting purposes, we generated a script to initialize DDR3 to use a 400MHz (instead of 533MHz) clock using the v1.9 Freescale Register Aid tool (latest as of 12/5/15).&amp;nbsp; We verified the 400MHz initialization script was indeed different from a 533MHz script generated by the same tool.&amp;nbsp; However, after using the 400MHz script to initialize DDR, the clock frequency remains at 533MHz by o-scope measurement (we saw this issue before with the old register scripting aid too).&amp;nbsp; Because the clock frequency does not change there is no way we can try a lower frequency for troubleshooting our DDR3.&amp;nbsp; Is there something additional that needs to be done in order to get the 400MHz clock frequency or is this an indication of a larger issue with our i.MX6Q?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2015 14:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466177#M73451</guid>
      <dc:creator>cbrust</dc:creator>
      <dc:date>2015-12-07T14:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q DDR3 clock problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466178#M73452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;generated script just calculates MMC/DDR settings but does not set CCM frequencies.&lt;/P&gt;&lt;P&gt;This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.&lt;/P&gt;&lt;P&gt;So there are no indication of any&amp;nbsp; issues with your i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 06:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466178#M73452</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-08T06:02:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q DDR3 clock problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466179#M73453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may create SR to get some example sources how to change frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 06:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466179#M73453</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-12-08T06:20:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q DDR3 clock problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466180#M73454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We figured we were missing something simple or making a bad assumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cliff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 12:21:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-DDR3-clock-problem/m-p/466180#M73454</guid>
      <dc:creator>cbrust</dc:creator>
      <dc:date>2015-12-08T12:21:12Z</dc:date>
    </item>
  </channel>
</rss>