<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using qt in I.MX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-qt-in-I-MX6UL/m-p/466110#M73426</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general it can use as discussed on meta-fsl-arm mailing list:&lt;/P&gt;&lt;P&gt;&lt;A href="http://comments.gmane.org/gmane.linux.embedded.yocto.meta-freescale/18128" title="http://comments.gmane.org/gmane.linux.embedded.yocto.meta-freescale/18128"&gt;Freescale OpenEmbedded/Yocto Layers discussion list ()&lt;/A&gt;&lt;/P&gt;&lt;P&gt;however it is not supported in official bsp, refer to attached Release Notes p.8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jun 2016 07:24:08 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-01T07:24:08Z</dc:date>
    <item>
      <title>Using qt in I.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-qt-in-I-MX6UL/m-p/466109#M73425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I.MX6UL has no accelerator for 2D/3D.&lt;/P&gt;&lt;P&gt;Does it mean that I.MX6UL can't use QT applications at all?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 07:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-qt-in-I-MX6UL/m-p/466109#M73425</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2016-06-01T07:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: Using qt in I.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-qt-in-I-MX6UL/m-p/466110#M73426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general it can use as discussed on meta-fsl-arm mailing list:&lt;/P&gt;&lt;P&gt;&lt;A href="http://comments.gmane.org/gmane.linux.embedded.yocto.meta-freescale/18128" title="http://comments.gmane.org/gmane.linux.embedded.yocto.meta-freescale/18128"&gt;Freescale OpenEmbedded/Yocto Layers discussion list ()&lt;/A&gt;&lt;/P&gt;&lt;P&gt;however it is not supported in official bsp, refer to attached Release Notes p.8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 07:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-qt-in-I-MX6UL/m-p/466110#M73426</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-01T07:24:08Z</dc:date>
    </item>
  </channel>
</rss>