<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Boot Linux from QSPI NOR</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Linux-from-QSPI-NOR/m-p/466087#M73419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am working on imx6UL evk board. I want to boot linux from QSPI flash by putting zImage, device tree &amp;amp; rfs on QSPI only. Is there any good tutorial available for the same? &lt;/P&gt;&lt;P&gt;Any help is highly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Apr 2016 17:43:06 GMT</pubDate>
    <dc:creator>nitigupta</dc:creator>
    <dc:date>2016-04-21T17:43:06Z</dc:date>
    <item>
      <title>Boot Linux from QSPI NOR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Linux-from-QSPI-NOR/m-p/466087#M73419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am working on imx6UL evk board. I want to boot linux from QSPI flash by putting zImage, device tree &amp;amp; rfs on QSPI only. Is there any good tutorial available for the same? &lt;/P&gt;&lt;P&gt;Any help is highly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 17:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Linux-from-QSPI-NOR/m-p/466087#M73419</guid>
      <dc:creator>nitigupta</dc:creator>
      <dc:date>2016-04-21T17:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Linux from QSPI NOR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Linux-from-QSPI-NOR/m-p/466088#M73420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Niti,&lt;/P&gt;&lt;P&gt;You could take a look at the following document, which explains how to change the boot source and considerations:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328196"&gt;Booting Linux from SATA on i.MX6Q SABRE AI.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You could also refer to a similar QSPI boot clarifications on Vybrid which use the same controller than the i.MX6X and verify what applies for the i.MX6UL:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309037"&gt;Parallel QuadSPI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 00:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Linux-from-QSPI-NOR/m-p/466088#M73420</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-04-22T00:39:35Z</dc:date>
    </item>
  </channel>
</rss>