<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6q dual HD display problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-dual-HD-display-problem/m-p/466021#M73409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maciej,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;The speed of i.MX6 LVDS serial ports is up to 165 Mpixels/sec for single channel or 85 Mpixels/sec for dual channel. So it allows&amp;nbsp; 1920x1200 at 60 fps for single channel and 1366x768 at 60 fps for dual channel.&lt;BR /&gt; &lt;BR /&gt; The default Android image supports dual display (LVDS + HDMI) by the following commands:&lt;BR /&gt; Under the U-Boot prompt, please set the following U-Boot environment var.&lt;BR /&gt; U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0:dev=ldb,LDBXGA, if=RGB666,bpp=16 fb0base=0x27b00000 video=mxcfb1:dev=hdmi,1920x1080M@60 fbmem=10M,28M&amp;nbsp; video=mxcfb2:off vmalloc=512M androidboot.console=ttymxc0&lt;BR /&gt; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt; Please also refer to &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93449"&gt;https://community.freescale.com/docs/DOC-93449&lt;/A&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/317168#317168"&gt;https://community.freescale.com/message/317168&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jan 2016 17:02:46 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2016-01-27T17:02:46Z</dc:date>
    <item>
      <title>imx6q dual HD display problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-dual-HD-display-problem/m-p/466020#M73408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm using IMX6-Quad processor with board that has dual-channel lvds and hdmi output. The problem that i couldn't resolv, is that when i setup dual-channel lvds output ( 1980x1020 ) i cannot use the hdmi output ( 1080p ). &lt;/P&gt;&lt;P&gt;The kernel that i'm using is the 3.14.38 &lt;/P&gt;&lt;P&gt;The linux distribution is not important.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone that use dual-channel lvds display with fullHD resolution with hdmi fullHD output ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;Maciej Kaźmierczak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2016 13:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-dual-HD-display-problem/m-p/466020#M73408</guid>
      <dc:creator>maciejka_miercz</dc:creator>
      <dc:date>2016-01-26T13:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q dual HD display problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-dual-HD-display-problem/m-p/466021#M73409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maciej,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;The speed of i.MX6 LVDS serial ports is up to 165 Mpixels/sec for single channel or 85 Mpixels/sec for dual channel. So it allows&amp;nbsp; 1920x1200 at 60 fps for single channel and 1366x768 at 60 fps for dual channel.&lt;BR /&gt; &lt;BR /&gt; The default Android image supports dual display (LVDS + HDMI) by the following commands:&lt;BR /&gt; Under the U-Boot prompt, please set the following U-Boot environment var.&lt;BR /&gt; U-Boot &amp;gt; setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0:dev=ldb,LDBXGA, if=RGB666,bpp=16 fb0base=0x27b00000 video=mxcfb1:dev=hdmi,1920x1080M@60 fbmem=10M,28M&amp;nbsp; video=mxcfb2:off vmalloc=512M androidboot.console=ttymxc0&lt;BR /&gt; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt; Please also refer to &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93449"&gt;https://community.freescale.com/docs/DOC-93449&lt;/A&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/317168#317168"&gt;https://community.freescale.com/message/317168&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 17:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-dual-HD-display-problem/m-p/466021#M73409</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-01-27T17:02:46Z</dc:date>
    </item>
  </channel>
</rss>