<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failure to create a image on uSD card using Windows MFG Tool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465864#M73352</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two micro-usb otg ports on the base board. One is USB-OTG (J1102) and one is USB-UART (J1901). When you using the MFGtool, there should be some messages output from the USB-UART one. And the board boot up, log message will output from the USB-UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't want to use MFGtool, you can use 'dd' command to program the SD card. You can find the instruction in the i.MX Linux User's Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, put your SD card into the USB card reader then program the u-boot to the SD card by this command.&lt;/P&gt;&lt;P&gt;$ sudo dd if=&amp;lt;U-Boot image&amp;gt; of=/dev/sdx bs=512 seek=2 conv=fsync&amp;nbsp; (where sdx is the device name of your card reader)&lt;/P&gt;&lt;P&gt;The first 1 KB of the SD/MMC card, which includes the partition table, is preserved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Dec 2015 08:19:42 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2015-12-08T08:19:42Z</dc:date>
    <item>
      <title>Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465859#M73347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running into a number of problems using the manufacturing tool.&amp;nbsp; I'm following the steps exactly as detailed in the "Getting Started" video and written guide.&amp;nbsp; Several of my co-conspirators with identical hardware are encountering the same problem.&amp;nbsp; When I run the VB script that ends in *sd2.vbs" the image creation fails during the writing of the root file system after the micro SD card is formatted.&amp;nbsp; Windows asks to format the micro SD card but that format fails.&amp;nbsp; I just close the dialog box.&amp;nbsp; The image creation gets past the formatting step and then fails.&amp;nbsp; I have tried a number of different micro SD card from different manufacturers.&amp;nbsp; I tired 8GB, 16GB and 64GB micro SD cards all with the same result.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2015 16:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465859#M73347</guid>
      <dc:creator>farangutan</dc:creator>
      <dc:date>2015-12-05T16:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465860#M73348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you tell me which BSP and board are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2015 08:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465860#M73348</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2015-12-07T08:27:43Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465861#M73349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jimmy&lt;/P&gt;&lt;P&gt;I used the i.mx6UL development kit (SOM + BB) that is featuring in the getting started video. &amp;nbsp;I'm not sure how to answer the BSP question. &amp;nbsp;The creation of the SD card is failing.&lt;/P&gt;&lt;P&gt;I downloaded the latest MFgTool software,&amp;nbsp;unpacked it on Windows 7 with 7Zip. &amp;nbsp;I tried to install and boot the image called "mfg2tool-yocto-mx-evk-sdcard-sd2.vbs"&lt;/P&gt;&lt;P&gt;The first part of creating the SD card seemed to work. &amp;nbsp;U-Boot and other DTLIB files were written on the SD card. The i.mx6UL processor then rebooted and a message appeared about formatting the SD card appeared on the MFgTool.&lt;/P&gt;&lt;P&gt;Also, a Windows dialog box opened asking to format the SD card which I found very surprising. &amp;nbsp;The Windows utility failed to format the card. &amp;nbsp;I restarted the entire MFgTool process from the beginning and just checked "cancel" when the Windows dialog box appeared. &amp;nbsp;&lt;/P&gt;&lt;P&gt;The creation of the SD card image continued for a few minutes and then a "writing" a root file system message appeared. &amp;nbsp;After 30 seconds, the progress bar on the Mfg Tool turns red and the MfgTool reports "failed".&lt;/P&gt;&lt;P&gt;Also, tried "&lt;STRONG&gt;qspi&lt;/STRONG&gt;.vbs" file. &amp;nbsp;The QSPI image was reported as written correctly by the MfgTool but when I tried to boot it (yes, the SW601 and SW602 on the SOM were set correctly) not Linux prompt appeared on the console.&lt;/P&gt;&lt;P&gt;Several other people boot on my team bought SOM+BB kits (all directly from Freescale). &amp;nbsp;All of us are encountering the same problem. &amp;nbsp;I apologize for being somewhat "stealthy" but I don't want my competitors to learn what we are doing.&lt;/P&gt;&lt;P&gt;Thanks for your help,Wayne&lt;/P&gt;&lt;P&gt;&amp;nbsp;"Non Impediti Ratione Cogitationis", -- unencumbered by rational thought!&lt;/P&gt;&lt;P&gt;      From: jimmychan &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt; To: Wayne Radochonski &amp;lt;wayne.radochonski@yahoo.com&amp;gt; &lt;/P&gt;&lt;P&gt; Sent: Monday, December 7, 2015 1:27 AM&lt;/P&gt;&lt;P&gt; Subject: Re:  - Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;|  &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;| &lt;/P&gt;&lt;P&gt;Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;reply from jimmychan in i.MX Community - View the full discussioncould you tell me which BSP and board are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread!&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Reply to this message by replying to this email, or go to the message on Freescale Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Start a new discussion in i.MX Community by email or at Freescale Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Following Failure to create a image on uSD card using Windows MFG Tool in these streams: Inbox&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  This email was sent by Freescale Community because you are a registered user.&lt;/P&gt;&lt;P&gt; You may unsubscribe instantly from Freescale Community, or adjust email frequency in your email preferences   |&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  |&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2015 12:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465861#M73349</guid>
      <dc:creator>farangutan</dc:creator>
      <dc:date>2015-12-07T12:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465862#M73350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you are using i.MX6UL EVK. This is the link of this board.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK" title="http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK"&gt;i.MX6ULtraLite Evaluation Kit|NXP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the proper images and mfgtool for i.MX6UL EVK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the BSP and demo image, you can download it from "Downloads" page under Board Support Packages.&lt;/P&gt;&lt;P&gt;For the MFGtool for 6UL, you can download it from "Downloads" page under Programmers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the details about all the steps of building BSP and how-to program the board, please read the user guide in L3.14.38_6ul_LINUX_DOCS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 03:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465862#M73350</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2015-12-08T03:54:55Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465863#M73351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jimmy&lt;/P&gt;&lt;P&gt;I followed all the steps in the documentation exactly. &amp;nbsp;Several other members of my team, all encountered the same&amp;nbsp;problem. &amp;nbsp;They followed the directions independently. &amp;nbsp;All of us had the same result. &amp;nbsp;The documentation makes no mention of the Windows formatting program ever running yet it does. &amp;nbsp;&lt;/P&gt;&lt;P&gt;We need to verify that our EVK hardware is working as step one. &amp;nbsp;Building a BSP comes later. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Understand that I'm trying to make both our organizations a success not be a difficult customer. &amp;nbsp;I just have no time to waste. &amp;nbsp;We have very limited time to get our product to market.&lt;/P&gt;&lt;P&gt;In the archive "mfgtools-with-rootfs.tar", these files were found:&lt;/P&gt;&lt;P&gt;mfgtool2-yocto-mx-evk-qspi-nor-n25q256a&lt;/P&gt;&lt;P&gt;mfgtool2-yocto-mx-evk-sdcard-ldo-sd1.vbsmfgtool2-yocto-mx-evk-sdcard-ldo-sd2.vbsmfgtool2-yocto-mx-evk-sdcard-ldo-sd3.vbsmfgtool2-yocto-mx-evk-sdcard-sd1.vbsmfgtool2-yocto-mx-evk-sdcard-sd2.vbsmfgtool2-yocto-mx-evk-sdcard-sd3.vbsmfgtool2-yocto-mx-evk-spi-nor.vbs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All of these files appear to be VB scripts that write an image onto an SD card or QSPI. &amp;nbsp;The VB script "mfgtool2-yocto-mx-evk-qspi-nor-n25q256a" claims to correctly write the QSPI. &amp;nbsp;When SW601 is set for QSPI boot (D1-D4 all off) and SW602 is set to internal boot (D1-On, D2-Off), Linux does not appear to boot. &amp;nbsp;Nothing appears on the serial console.&lt;/P&gt;&lt;P&gt;Using the MFgTool, the mfgtool2-yocto-mx-evk-sdcard-sd2.vbs script fails to write the SD card. &amp;nbsp;The write fails during "Writing Root File System" step. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Our team ordered five i.mx6UL EVKs from Freescale directly. &amp;nbsp;All of these boards behave identically. &amp;nbsp;QSPI image does not appear to work. &amp;nbsp;All of the other images fail during the write of the SD card.&lt;/P&gt;&lt;P&gt;What is the difference between mfgtool2-yocto-mx-evk-sdcard-ldo-sd2.vbs and mfgtool2-yocto-mx-evk-sdcard-sd2.vbs? &amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a procedure for creating an SD card under Linux directly, that does not use the MFGTool program?&lt;/P&gt;&lt;P&gt;The problem could be bad EVK hardware, our understanding of the procedure (but it seems very straightforward) for writing an SD card or just that the MFGTool isn't working, &amp;nbsp;All of the failures to write the SD card occurred when running MFGTool under Win7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can't provide any more help, then I need to know how to escalate this problem. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Our schedule is being impacted by the inability of the EVK to boot Linux. An order of 100K/pieces a year is continent upon us getting the EVK working, followed by our own target hardware. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wayne&amp;nbsp;"Non Impediti Ratione Cogitationis", -- unencumbered by rational thought!&lt;/P&gt;&lt;P&gt;      From: jimmychan &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt; To: Wayne Radochonski &amp;lt;wayne.radochonski@yahoo.com&amp;gt; &lt;/P&gt;&lt;P&gt; Sent: Monday, December 7, 2015 8:55 PM&lt;/P&gt;&lt;P&gt; Subject: Re:  - Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;|  &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;| &lt;/P&gt;&lt;P&gt;Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;reply from jimmychan in i.MX Community - View the full discussionI think you are using i.MX6UL EVK. This is the link of this board.i.MX6ULtraLite Evaluation Kit|NXP &amp;nbsp;Are you using the proper images and mfgtool for i.MX6UL EVK?&amp;nbsp;For the BSP and demo image, you can download it from "Downloads" page under Board Support Packages.For the MFGtool for 6UL, you can download it from "Downloads" page under Programmers.&amp;nbsp;For the details about all the steps of building BSP and how-to program the board, please read the user guide in L3.14.38_6ul_LINUX_DOCS.&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread!&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Reply to this message by replying to this email, or go to the message on NXP Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Start a new discussion in i.MX Community by email or at NXP Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Following Failure to create a image on uSD card using Windows MFG Tool in these streams: Inbox&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  This email was sent by NXP Community because you are a registered user.&lt;/P&gt;&lt;P&gt; You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 06:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465863#M73351</guid>
      <dc:creator>farangutan</dc:creator>
      <dc:date>2015-12-08T06:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465864#M73352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two micro-usb otg ports on the base board. One is USB-OTG (J1102) and one is USB-UART (J1901). When you using the MFGtool, there should be some messages output from the USB-UART one. And the board boot up, log message will output from the USB-UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't want to use MFGtool, you can use 'dd' command to program the SD card. You can find the instruction in the i.MX Linux User's Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, put your SD card into the USB card reader then program the u-boot to the SD card by this command.&lt;/P&gt;&lt;P&gt;$ sudo dd if=&amp;lt;U-Boot image&amp;gt; of=/dev/sdx bs=512 seek=2 conv=fsync&amp;nbsp; (where sdx is the device name of your card reader)&lt;/P&gt;&lt;P&gt;The first 1 KB of the SD/MMC card, which includes the partition table, is preserved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 08:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465864#M73352</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2015-12-08T08:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: Failure to create a image on uSD card using Windows MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465865#M73353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jimmy&lt;/P&gt;&lt;P&gt;Thanks for the very prompt&amp;nbsp;response and your patience. &amp;nbsp;The EVK/SOM is causing a number of headaches for all of us. &amp;nbsp;The first step for us to have confidence that our EVK hardware is actually working by booting a Linux image that Freescale has created. &amp;nbsp;We will try using "dd" to create a SD card image.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are other i.mx6UL SOMs available but they aren't quite ready for delivery. If we don't make progress with the EVK soon, we will try a SOM from another vendor. &amp;nbsp;We like the i.mx6UL MPU, the EVK not so much. &amp;nbsp;If Freescale ever spins the SOM, please get rid of that awful micro SD connector on the SOM in favor of eMMC (ok, enough whining).&lt;/P&gt;&lt;P&gt;None of the Freescale documentation mentions the Win7 format utility actually running. &amp;nbsp;Yet we see that happening consistently. &amp;nbsp;Is the Win7 formatting utility expected to run when the MfgTool is used?&lt;/P&gt;&lt;P&gt;Thanks again for your help. &amp;nbsp;I will let you know the results of creating an image using "dd".&lt;/P&gt;&lt;P&gt;Wayne&amp;nbsp;"Non Impediti Ratione Cogitationis", -- unencumbered by rational thought!&lt;/P&gt;&lt;P&gt;      From: jimmychan &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt; To: Wayne Radochonski &amp;lt;wayne.radochonski@yahoo.com&amp;gt; &lt;/P&gt;&lt;P&gt; Sent: Tuesday, December 8, 2015 1:20 AM&lt;/P&gt;&lt;P&gt; Subject: Re:  - Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;|  &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;| &lt;/P&gt;&lt;P&gt;Failure to create a image on uSD card using Windows MFG Tool&lt;/P&gt;&lt;P&gt;reply from jimmychan in i.MX Community - View the full discussionThere are two micro-usb otg ports on the base board. One is USB-OTG (J1102) and one is USB-UART (J1901). When you using the MFGtool, there should be some messages output from the USB-UART one. And the board boot up, log message will output from the USB-UART.&amp;nbsp;If you don't want to use MFGtool, you can use 'dd' command to program the SD card. You can find the instruction in the i.MX Linux User's Guide.&amp;nbsp;For example, put your SD card into the USB card reader then program the u-boot to the SD card by this command.$ sudo dd if=&amp;lt;U-Boot image&amp;gt; of=/dev/sdx bs=512 seek=2 conv=fsync&amp;nbsp; (where sdx is the device name of your card reader)The first 1 KB of the SD/MMC card, which includes the partition table, is preserved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Did your question get answered? If so, say thanks by clicking Correct Answer in the community thread!&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Reply to this message by replying to this email, or go to the message on NXP Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Start a new discussion in i.MX Community by email or at NXP Community&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;Following Failure to create a image on uSD card using Windows MFG Tool in these streams: Inbox&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  This email was sent by NXP Community because you are a registered user.&lt;/P&gt;&lt;P&gt; You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences   |&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;  |&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 13:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-to-create-a-image-on-uSD-card-using-Windows-MFG-Tool/m-p/465865#M73353</guid>
      <dc:creator>farangutan</dc:creator>
      <dc:date>2015-12-08T13:37:47Z</dc:date>
    </item>
  </channel>
</rss>