<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECSPI2_SS1 not working properly in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465765#M73339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in DTS file which is using imx6q-pinfun.h is defined as :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__EIM_LBA_B&amp;nbsp;&amp;nbsp; 0x108 0x41c 0x000 0x0 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__IPU1_DI1_PIN17&amp;nbsp;&amp;nbsp; 0x108 0x41c 0x000 0x1 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__ECSPI2_SS1&amp;nbsp; 0x108 0x41c 0x820 0x2 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__GPIO2_IO27&amp;nbsp; 0x108 0x41c 0x820 0x2 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__SRC_BOOT_CFG26 0x108 0x41c 0x000 0x7 0x0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my dtsi/dts files if i use&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_SD4_DAT1__PWM3_OUT 0x1b0b1 then SD4_DAT1 should be linked to PWM3 _OUT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and if i use&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_SD4_DAT1__SD4_DATA1&amp;nbsp; 0x17059 then it should be linked automatically to SD4_DATA1 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or do we need to do some setting for linking of SD4_DAT1 (in software perspective)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from IMX6DQ reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default mux mode of SD4_DAT1 is set to GPIO (GPIO2_IO29)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should we do to get SD4_DAT1 to PWM3_OUT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Dec 2015 09:28:01 GMT</pubDate>
    <dc:creator>srinivasaporam</dc:creator>
    <dc:date>2015-12-15T09:28:01Z</dc:date>
    <item>
      <title>ECSPI2_SS1 not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465763#M73337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are working on a IMX6 board where we have attached a sensor through SPI to ECSPI2. the chip select ECSPI2_SS1 we have choosen as EIM_LBA as per the reference manual. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; This EIM_LBA corresponds to GPIO2_IO27 (GPIO59 ((2-1)*32+27)).&amp;nbsp; From our application we are making this GPIO59 to high and low but it is not happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where as we have cross checked it with another SPI (ECSPI1 with SS0) where ECSPI1_SS0 is taken as EIM_EB2 whose respective GPIO is GPIO2_IO30&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which is GPIO62. When we are making GPIO62 high and low and probing at ECSPI1_SS0 we are getting the signal high and low as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is problem with ECSPI2_SS1 (same is the problem with ECSPI2_SS0 also). what mistake we are doing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2015 05:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465763#M73337</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-12-07T05:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI2_SS1 not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465764#M73338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;Please check if iomuxc section of ecspi2 is correctly describes the SS pin function as GPIO.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 08:28:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465764#M73338</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-12-10T08:28:58Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI2_SS1 not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465765#M73339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in DTS file which is using imx6q-pinfun.h is defined as :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__EIM_LBA_B&amp;nbsp;&amp;nbsp; 0x108 0x41c 0x000 0x0 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__IPU1_DI1_PIN17&amp;nbsp;&amp;nbsp; 0x108 0x41c 0x000 0x1 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__ECSPI2_SS1&amp;nbsp; 0x108 0x41c 0x820 0x2 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__GPIO2_IO27&amp;nbsp; 0x108 0x41c 0x820 0x2 0x0&lt;/P&gt;&lt;P&gt;#define MX6QDL_PAD_EIM_LBA__SRC_BOOT_CFG26 0x108 0x41c 0x000 0x7 0x0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my dtsi/dts files if i use&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_SD4_DAT1__PWM3_OUT 0x1b0b1 then SD4_DAT1 should be linked to PWM3 _OUT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and if i use&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_SD4_DAT1__SD4_DATA1&amp;nbsp; 0x17059 then it should be linked automatically to SD4_DATA1 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or do we need to do some setting for linking of SD4_DAT1 (in software perspective)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from IMX6DQ reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default mux mode of SD4_DAT1 is set to GPIO (GPIO2_IO29)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should we do to get SD4_DAT1 to PWM3_OUT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 09:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI2-SS1-not-working-properly/m-p/465765#M73339</guid>
      <dc:creator>srinivasaporam</dc:creator>
      <dc:date>2015-12-15T09:28:01Z</dc:date>
    </item>
  </channel>
</rss>