<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6UL LDO bypass in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465284#M73247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version are you reviewing of the Reference Manual,?&amp;nbsp; because in the latest available on the web site REV 0, 08/2015. It states :&lt;/P&gt;&lt;P data-canvas-width="813.4466666666667" style="font-size: 23.3333px; font-family: serif;"&gt;"If the &lt;STRONG&gt;external&lt;/STRONG&gt; SRC_POR_B signal is used to control the processor POR, SRC_POR_B&lt;/P&gt;&lt;P data-canvas-width="806.9133333333336" style="font-size: 23.3333px; font-family: serif;"&gt;must remain low (asserted) until the VDD_ARM_CAP and VDD_SOC_CAP supplies&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;are stable."&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="807.52" style="font-size: 23.3333px; font-family: serif;"&gt;"If the internal POR function is used, the following power supply requirements must be&lt;/P&gt;&lt;P data-canvas-width="41.486666666666665" style="font-size: 23.3333px; font-family: serif;"&gt;met:&lt;/P&gt;&lt;P data-canvas-width="754.9966666666667" style="font-size: 23.3333px; font-family: serif;"&gt;• VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source, or&lt;/P&gt;&lt;P data-canvas-width="799.0733333333334" style="font-size: 23.3333px; font-family: serif;"&gt;• VDD_SOC_IN can be supplied before VDD_ARM_IN with a maximum delay of 1ms"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes if you supply 1.2V to the VDD_SOC_IN and VDD_ARM_IN then device should be working correctly!. and out of reset.&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Feb 2016 16:35:54 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2016-02-17T16:35:54Z</dc:date>
    <item>
      <title>i.MX6UL LDO bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465283#M73246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing a board with the i.MX6 UltraLite processor. I want to power the CPU using a 1.2V regulator, bypassing the internal LDO_ARM and LDO_SOC regulators. However, the reference manual states that the internal POR module will hold the CPU in reset until the VDD_SOC_CAP supply is "valid." The LDO_SOC regulator is set to 1.15 volts by default, which does not give the LDO enough overhead given a 1.2V input: the dropout voltage is 150mV. The datasheet states an operating VDD_SOC_IN voltage of 1.15-1.3V, with the internal LDO bypassed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, if I supply 1.2V to the VDD_SOC_IN, with intent to bypass the internal regulator, will the internal POR module ever bring the CPU out of reset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, if it does, what is the easiest way to bypass the internal LDO?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 14:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465283#M73246</guid>
      <dc:creator>samchinnery</dc:creator>
      <dc:date>2016-02-17T14:08:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL LDO bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465284#M73247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version are you reviewing of the Reference Manual,?&amp;nbsp; because in the latest available on the web site REV 0, 08/2015. It states :&lt;/P&gt;&lt;P data-canvas-width="813.4466666666667" style="font-size: 23.3333px; font-family: serif;"&gt;"If the &lt;STRONG&gt;external&lt;/STRONG&gt; SRC_POR_B signal is used to control the processor POR, SRC_POR_B&lt;/P&gt;&lt;P data-canvas-width="806.9133333333336" style="font-size: 23.3333px; font-family: serif;"&gt;must remain low (asserted) until the VDD_ARM_CAP and VDD_SOC_CAP supplies&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;are stable."&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="807.52" style="font-size: 23.3333px; font-family: serif;"&gt;"If the internal POR function is used, the following power supply requirements must be&lt;/P&gt;&lt;P data-canvas-width="41.486666666666665" style="font-size: 23.3333px; font-family: serif;"&gt;met:&lt;/P&gt;&lt;P data-canvas-width="754.9966666666667" style="font-size: 23.3333px; font-family: serif;"&gt;• VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source, or&lt;/P&gt;&lt;P data-canvas-width="799.0733333333334" style="font-size: 23.3333px; font-family: serif;"&gt;• VDD_SOC_IN can be supplied before VDD_ARM_IN with a maximum delay of 1ms"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes if you supply 1.2V to the VDD_SOC_IN and VDD_ARM_IN then device should be working correctly!. and out of reset.&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P data-canvas-width="94.59333333333332" style="font-size: 23.3333px; font-family: serif;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 16:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465284#M73247</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2016-02-17T16:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL LDO bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465285#M73248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if it's not too much trouble, what is the best way to disable the LDO_ARM regulator? Is it possible to disable it early in the boot prcess, or must the program image be loaded first?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 18:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465285#M73248</guid>
      <dc:creator>samchinnery</dc:creator>
      <dc:date>2016-02-17T18:30:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL LDO bypass</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465286#M73249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From my experience it is better at the boot process.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 18:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-LDO-bypass/m-p/465286#M73249</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2016-02-19T18:43:51Z</dc:date>
    </item>
  </channel>
</rss>