<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: U-Boot version for i.MX6Q customized board from refrence Sabreauto board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-version-for-i-MX6Q-customized-board-from-refrence/m-p/464717#M73143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please use Chapter 1 (Porting U-Boot from an i.MX 6/7 Reference&lt;/P&gt;&lt;P&gt;Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A href="https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Informat…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 02:45:11 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-02-18T02:45:11Z</dc:date>
    <item>
      <title>U-Boot version for i.MX6Q customized board from refrence Sabreauto board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-version-for-i-MX6Q-customized-board-from-refrence/m-p/464716#M73142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to clone official/correct U-boot version for i.MX6Q Sabreauto(reference) board to customize a similar board.&lt;/P&gt;&lt;P&gt;Please provide me a working source link, I've seen in community that different versions are being used like U-boot 2009.08 &amp;amp; 2015.04 etc.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am little confused and want to make sure I'm using correct working version,so please help.&lt;/P&gt;&lt;P&gt;And also while using the following command to clone fsl-arm-yocto-bsp i'm getting a fatal error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fatal: unable to connect to git.freescale.com:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Does the above BSP contain u-boot alone or any additional drivers? i guess no linux kernel too?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I like to build only U-boot image for my customized board, so do you recommend to use yocto project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 13:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-version-for-i-MX6Q-customized-board-from-refrence/m-p/464716#M73142</guid>
      <dc:creator>maheshkumarkoda</dc:creator>
      <dc:date>2016-02-17T13:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot version for i.MX6Q customized board from refrence Sabreauto board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-version-for-i-MX6Q-customized-board-from-refrence/m-p/464717#M73143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please use Chapter 1 (Porting U-Boot from an i.MX 6/7 Reference&lt;/P&gt;&lt;P&gt;Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A href="https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz&amp;amp;Parent_nodeId=1337637154535695831062&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Supporting%20Informat…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 02:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-version-for-i-MX6Q-customized-board-from-refrence/m-p/464717#M73143</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-18T02:45:11Z</dc:date>
    </item>
  </channel>
</rss>