<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRecommended NAND driver for i.MX51 (Linux OS)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recommended-NAND-driver-for-i-MX51-Linux-OS/m-p/179128#M7302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am encountering file system corruption issues (UBIFS and JFFS2) and am attempting to determine the root cause. &amp;nbsp;In both cases the file systems are trashed during stress testing of our system software upgrade process. &amp;nbsp;In both cases, the file system is mounted with the -o sync option in an attempt to mitigate any write buffering issues associated with either file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;System Info:&lt;/P&gt;&lt;P&gt;current driver: Kernel Config -&amp;gt; Device Drivers -&amp;gt; MTD Support -&amp;gt; MXC NAND Version 3 support&lt;/P&gt;&lt;P&gt;NAND Chip: Micron MT29F4G08 (slc)&lt;/P&gt;&lt;P&gt;BSP: 11.01 (I think. &amp;nbsp;I inherited this environment in a "transitional" state)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed that there is an option for selecting an "i.MX NAND Flash Controller driver" in the kernel config but can't seem to locate any information on it. &amp;nbsp;Can anyone provide recommendations for using one over the other? &amp;nbsp;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Russ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2012 15:06:03 GMT</pubDate>
    <dc:creator>RussellZuck</dc:creator>
    <dc:date>2012-08-02T15:06:03Z</dc:date>
    <item>
      <title>Recommended NAND driver for i.MX51 (Linux OS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recommended-NAND-driver-for-i-MX51-Linux-OS/m-p/179128#M7302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am encountering file system corruption issues (UBIFS and JFFS2) and am attempting to determine the root cause. &amp;nbsp;In both cases the file systems are trashed during stress testing of our system software upgrade process. &amp;nbsp;In both cases, the file system is mounted with the -o sync option in an attempt to mitigate any write buffering issues associated with either file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;System Info:&lt;/P&gt;&lt;P&gt;current driver: Kernel Config -&amp;gt; Device Drivers -&amp;gt; MTD Support -&amp;gt; MXC NAND Version 3 support&lt;/P&gt;&lt;P&gt;NAND Chip: Micron MT29F4G08 (slc)&lt;/P&gt;&lt;P&gt;BSP: 11.01 (I think. &amp;nbsp;I inherited this environment in a "transitional" state)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed that there is an option for selecting an "i.MX NAND Flash Controller driver" in the kernel config but can't seem to locate any information on it. &amp;nbsp;Can anyone provide recommendations for using one over the other? &amp;nbsp;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Russ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2012 15:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recommended-NAND-driver-for-i-MX51-Linux-OS/m-p/179128#M7302</guid>
      <dc:creator>RussellZuck</dc:creator>
      <dc:date>2012-08-02T15:06:03Z</dc:date>
    </item>
  </channel>
</rss>