<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using i.MX25's integrated UTMI PHY in device mode without Vbus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX25-s-integrated-UTMI-PHY-in-device-mode-without-Vbus/m-p/179060#M7292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We're planning to use our custom board with i.MX25 in USB device mode but unfortunately we haven't routed out the Vbus pin so here goes my question:&lt;/P&gt;&lt;P&gt;What is needed to actually put the integrated OTG controller in device mode and to start communication? I've disabled the vbus handling logic and made sure the RUN_STOP bit is unset but i still can't see a pull-up on a USB data line, so no communication is possible.&lt;/P&gt;&lt;P&gt;Using upstream kernel here of course.&lt;/P&gt;&lt;P&gt;The documentation about the integrated UTMI PHY seems to be lacking in this regard, so can anybody please enlighten me?&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2011 07:41:23 GMT</pubDate>
    <dc:creator>PaulFertser</dc:creator>
    <dc:date>2011-10-21T07:41:23Z</dc:date>
    <item>
      <title>Using i.MX25's integrated UTMI PHY in device mode without Vbus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX25-s-integrated-UTMI-PHY-in-device-mode-without-Vbus/m-p/179060#M7292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We're planning to use our custom board with i.MX25 in USB device mode but unfortunately we haven't routed out the Vbus pin so here goes my question:&lt;/P&gt;&lt;P&gt;What is needed to actually put the integrated OTG controller in device mode and to start communication? I've disabled the vbus handling logic and made sure the RUN_STOP bit is unset but i still can't see a pull-up on a USB data line, so no communication is possible.&lt;/P&gt;&lt;P&gt;Using upstream kernel here of course.&lt;/P&gt;&lt;P&gt;The documentation about the integrated UTMI PHY seems to be lacking in this regard, so can anybody please enlighten me?&lt;/P&gt;&lt;P&gt;TIA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2011 07:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX25-s-integrated-UTMI-PHY-in-device-mode-without-Vbus/m-p/179060#M7292</guid>
      <dc:creator>PaulFertser</dc:creator>
      <dc:date>2011-10-21T07:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX25's integrated UTMI PHY in device mode without Vbus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX25-s-integrated-UTMI-PHY-in-device-mode-without-Vbus/m-p/179061#M7293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd be interested in an answer to this question.&amp;nbsp; I am attempting to use the OTG port on an i.MX6Q as a device using the&amp;nbsp; UTMI PHY in the 1.1.0 BSP.&amp;nbsp; The VBUS is not powered locally as it is in SABRE boards.&amp;nbsp; The OTG port goes into low-power suspend mode on boot.&amp;nbsp; It does not respond to calls to wakeup via the sysfs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2013 18:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX25-s-integrated-UTMI-PHY-in-device-mode-without-Vbus/m-p/179061#M7293</guid>
      <dc:creator>kitz36</dc:creator>
      <dc:date>2013-03-06T18:02:21Z</dc:date>
    </item>
  </channel>
</rss>