<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SATA corruption in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463595#M72893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Hi Karan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I have the same problem of firmware getting corrupted with sata boot in imx6q board, whether have you got any clues??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Ambika&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jul 2016 11:35:47 GMT</pubDate>
    <dc:creator>ambika</dc:creator>
    <dc:date>2016-07-04T11:35:47Z</dc:date>
    <item>
      <title>SATA corruption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463592#M72890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;We have custom boards with imx6 quad processor with android jelly bean running on 3.0.35 kernel with SATA boot , size 30 gb .&amp;nbsp; After using the board for some time we are getting a SATA corruption messages, the errors are different for different boards, like eg&lt;/P&gt;&lt;H5&gt;&lt;SPAN style="color: #606060;"&gt;1-&amp;gt;&lt;/SPAN&gt;&lt;/H5&gt;&lt;P&gt;&lt;EM&gt;EXT4-fs error (device sda4): ext4_lookup:1044: inode #22: comm er.ServerThread: deleted inode referenced: 69&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Aborting journal on device sda4-8.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Kernel panic - not syncing: EXT4-fs (device sda4): panic forced after error&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CPU0: stopping&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[&amp;lt;c0131f84&amp;gt;] (unwind_backtrace+0x0/0x138) from [&amp;lt;c01243a8&amp;gt;] (do_IPI+0x1d4/0x208)&lt;/EM&gt;&lt;/P&gt;&lt;H5&gt;2-&amp;gt; &lt;/H5&gt;&lt;P&gt;&lt;EM&gt;ata1.00: exception Emask 0x1 SAct 0x1f SErr 0x0 action 0x6 frozen&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ata1.00: irq_stat 0x40000000&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ata1.00: cmd 60/08:00:00:90:84/00:00:02:00:00/40 tag 0 ncq 4096 in&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; res 40/00:18:60:e5:80/00:00:02:00:00/40 Emask 0x1 (device error)&lt;/EM&gt;&lt;/P&gt;&lt;H5&gt;3-&amp;gt;&lt;/H5&gt;&lt;P&gt;&lt;EM&gt;DVFS driver module loaded&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;rtc-m41t80 0-0068: setting system clock to 2055-09-11 10:21:10 UTC (2704270870)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Freeing init memory: 1136K&lt;/EM&gt;&lt;/P&gt;&lt;H5&gt;4-&amp;gt;&lt;/H5&gt;&lt;P&gt;&lt;EM&gt;binder: 4716:4716 transaction failed 29189, size 80-4&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;binder: 4716:4716 transaction failed 29189, size 212-4&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We getting stuck in this error. Due to these errors the displays hangs at splash screen with no android UI prompt .All the errors indicate that the SATA cards are getting corrupted. Is there any error with the JB android /&amp;nbsp; kernel/ anything&amp;nbsp; which is causing this corruption?&lt;/P&gt;&lt;P&gt;Kindly advice , also suggest solutions if any.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2016 12:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463592#M72890</guid>
      <dc:creator>karanbhagoji</dc:creator>
      <dc:date>2016-04-20T12:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: SATA corruption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463593#M72891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;corruption may be caused by sudden turn of power supplies,&lt;/P&gt;&lt;P&gt;recommended to use linux poweroff command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 00:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463593#M72891</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-21T00:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: SATA corruption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463594#M72892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;Agreed that the sudden turn turn off of power supplies may be&amp;nbsp; an issue here, but its not always the case, the device boots &lt;/P&gt;&lt;P&gt;after an abrupt power supply failure I have already tried to turn off the power supply abruptly many times, but the SATA card is not getting corrupted..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest any way to overcome this corruption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 09:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463594#M72892</guid>
      <dc:creator>karanbhagoji</dc:creator>
      <dc:date>2016-04-21T09:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: SATA corruption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463595#M72893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Hi Karan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I have the same problem of firmware getting corrupted with sata boot in imx6q board, whether have you got any clues??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Ambika&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 11:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463595#M72893</guid>
      <dc:creator>ambika</dc:creator>
      <dc:date>2016-07-04T11:35:47Z</dc:date>
    </item>
    <item>
      <title>Re: SATA corruption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463596#M72894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ambika ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late reply , but the above&amp;nbsp; suggestion is&amp;nbsp; true , it is due to improper power supply and etc. Abrupt power off after long time is the main reason as the journalling is not updated, and hence may lead to sata corruption, also to add , during power off if the journalling regions are corrupt then there is no way to update the same and hence error. Also recommend to check the connectors for loose connections .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 18:01:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SATA-corruption/m-p/463596#M72894</guid>
      <dc:creator>karanbhagoji</dc:creator>
      <dc:date>2016-08-08T18:01:11Z</dc:date>
    </item>
  </channel>
</rss>