<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463018#M72790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to install these services (ssh, etc) into the system you are running on the board.&lt;/P&gt;&lt;P&gt;For example you can add openssh-server package there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Dec 2015 11:41:32 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2015-12-15T11:41:32Z</dc:date>
    <item>
      <title>Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463017#M72789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am new on the MCIMX6UL-EVK and Processor expert software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to complete few task using processor expert software &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-make a hello world test project using arm cross compiler.&lt;/P&gt;&lt;P&gt;2-run this hello world remotely using linux on MCIMX6UL board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have completed first step but when i am trying to connect my board through SSH type connection the following error message is coming after entering user name and password-&lt;/P&gt;&lt;P&gt;&lt;STRONG style="text-decoration: underline;"&gt;Failed to connect SFTP subsystem: Remote host may not have sftp-server installed : java.io.IOException: inputstream is closed&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is how many types of remote connection is possible to run my code.and also tell me that how i can i do SSH connection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;before run my code i did the necessary required things like -&lt;/P&gt;&lt;P&gt;i have downloaded the fsl-image-gui-x11-imx6ulevk.sdcard linux image to SD card and set my board to SD card mode and then connect my board to ethernet cable.On terminal(Tera term) i have seen the Linux was booting but OpenSSH and Sftp was unable to install on that linux. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;Sirraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 10:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463017#M72789</guid>
      <dc:creator>sirrajrai</dc:creator>
      <dc:date>2015-12-04T10:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463018#M72790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to install these services (ssh, etc) into the system you are running on the board.&lt;/P&gt;&lt;P&gt;For example you can add openssh-server package there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 11:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463018#M72790</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-12-15T11:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463019#M72791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for ur reply &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;actually i had given these command on terminal to install openssh server(sudo apt-get install openssh-server) but it failed to install it.I faced error like&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;no&amp;nbsp; 'sudo' command found&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;no 'apt-get'&amp;nbsp; command found&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to this i am unable to install anything in rootfs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i searched on net but didn't find necessary things so plz tell me how can i install openssh and update in &lt;/P&gt;&lt;P&gt;freescale linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using Xilinx SDK for &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;MCIMX6UL board to load .elf file but finally i have to use processor expert so plz tell me how i can resolve error of apt-get and sudo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;Sirraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 09:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463019#M72791</guid>
      <dc:creator>sirrajrai</dc:creator>
      <dc:date>2015-12-29T09:24:35Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to Run On MCIMX6UL-EVK board remotely using processor Expert Software?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463020#M72792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this problem resolved?.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I too have a similar&amp;nbsp;condition.&lt;/P&gt;&lt;P&gt;We have two NXP, S32v23 board. Step followed:&lt;/P&gt;&lt;P&gt;1. Boot the board with the default SD card.&lt;/P&gt;&lt;P&gt;2. Use eclipse to create a new remote&amp;nbsp;connection to the board using SSH type.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This result in error.&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;Failed to connect SFTP subsystem: Remote host may not have &lt;/EM&gt;sftp&lt;EM&gt;-server &lt;/EM&gt;installed :&lt;EM&gt; java.io.IOException&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;I have tried connecting via putty and is able to get the prompt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How/What are the settings for the S32 studio to get the remote connection on the default boot-image of the board?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Feb 2019 15:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-able-to-Run-On-MCIMX6UL-EVK-board-remotely-using-processor/m-p/463020#M72792</guid>
      <dc:creator>krishnakumar_ma</dc:creator>
      <dc:date>2019-02-08T15:26:05Z</dc:date>
    </item>
  </channel>
</rss>