<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6SX: VADC: force video standard in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-force-video-standard/m-p/462858#M72759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I did not try this yet, but if you look at the vadc driver, it has a dev_init function. This function initializes almost every parameters for the block to work. If you don't want it to automatically sense the signal format/mode, then you can disable those codes and force the module to work in you desired mode with appropriate parameters for that mode. Not try yet but must be working, I guess.&lt;/P&gt;&lt;P&gt;Good luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 06:13:00 GMT</pubDate>
    <dc:creator>davidtrinh</dc:creator>
    <dc:date>2015-12-09T06:13:00Z</dc:date>
    <item>
      <title>iMX6SX: VADC: force video standard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-force-video-standard/m-p/462857#M72758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the integrated video-adc of the iMX6 SoloX. In both U-Boot and Linux Kernel the VADC performs an auto-detection of the video-standard (PAL/NTSC). I would like to have that pre-configured to save time and to handle weak/noisy signals better. How can I do that? I checked the documentation and found the "Manual Override (VDEC_MANOVR)" register, but the documentation is very minimalistic. I guess the "pal_override" and "pal_manual" flags are supposed to do that but I don't fully understand how. Unfortunately both UBoot and linux-kernel don't use this register at all so there is also no way to look it up.&lt;/P&gt;&lt;P&gt;Long story short: how do I force the VADC to use PAL or NTSC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 13:05:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-force-video-standard/m-p/462857#M72758</guid>
      <dc:creator>JohnDoe1z</dc:creator>
      <dc:date>2015-12-04T13:05:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX: VADC: force video standard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-force-video-standard/m-p/462858#M72759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I did not try this yet, but if you look at the vadc driver, it has a dev_init function. This function initializes almost every parameters for the block to work. If you don't want it to automatically sense the signal format/mode, then you can disable those codes and force the module to work in you desired mode with appropriate parameters for that mode. Not try yet but must be working, I guess.&lt;/P&gt;&lt;P&gt;Good luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 06:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-VADC-force-video-standard/m-p/462858#M72759</guid>
      <dc:creator>davidtrinh</dc:creator>
      <dc:date>2015-12-09T06:13:00Z</dc:date>
    </item>
  </channel>
</rss>