<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6ULEVK remote debug with eclipse</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULEVK-remote-debug-with-eclipse/m-p/462755#M72748</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf" title="http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;and sect.6.3. Debug Linux kernel code AN5229&lt;/P&gt;&lt;P&gt;ARM DS-5 Development Studio Debug i.MX6UL-EVK&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf" title="http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jun 2016 01:39:01 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-01T01:39:01Z</dc:date>
    <item>
      <title>IMX6ULEVK remote debug with eclipse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULEVK-remote-debug-with-eclipse/m-p/462754#M72747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to linux development. So I managed to create a custom linux and a toolchain with yocto and build a "hello world" on eclipse but I can't remote debug it. On eclipse, I tried debugging with gdbserver running on the target but it is way too slow. Then, I tried the direct remote debugger plugin from eclipse marketplace that get stuck at 57% and returns&amp;nbsp; the error "Could not start gdb on the remote host by ssh" when canceling. GDB is correctly installed on the target and I can launch it in a ssh terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My configuration :&lt;/P&gt;&lt;P&gt;Eclipse luna for linux&lt;/P&gt;&lt;P&gt;Ubuntu 16.04 running inside virtualbox on Windows 7&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion ? Is eclipse the best tool to develop linux applications on IMX6UL ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 14:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULEVK-remote-debug-with-eclipse/m-p/462754#M72747</guid>
      <dc:creator>YodaC</dc:creator>
      <dc:date>2016-05-30T14:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULEVK remote debug with eclipse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULEVK-remote-debug-with-eclipse/m-p/462755#M72748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf" title="http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN4553.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;and sect.6.3. Debug Linux kernel code AN5229&lt;/P&gt;&lt;P&gt;ARM DS-5 Development Studio Debug i.MX6UL-EVK&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf" title="http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 01:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULEVK-remote-debug-with-eclipse/m-p/462755#M72748</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-01T01:39:01Z</dc:date>
    </item>
  </channel>
</rss>