<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: ODT setting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting/m-p/462735#M72746</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ODT settings of IOMUX are for the DDR Address and control pins, &lt;/P&gt;&lt;P&gt;and the ODT settings of MMDCx_MPODTCTRL are for the Data bus (by byte group).&lt;/P&gt;&lt;P&gt;So you can controls the ODT value for each byte group by the ODTx_INT_RES.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 00:26:11 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-05-12T00:26:11Z</dc:date>
    <item>
      <title>ODT setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting/m-p/462734#M72745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have&amp;nbsp; successfully finished SI and timing closure using Hyperlynx 9.3 simulation tool. The tool requires&lt;/P&gt;&lt;P&gt;me to enable (ddr3_odt_t60_sel11_mi) ODT settings for read accesses from the memory to the MMDC controller. I want to know if this is accomplished in the MPODTCTRL register (0x021B01818) or in a IOMUX_SW_PAD_CTL_PAD_DRAM_xxxx register? Also in the Programming AID Ver 1.9 the MPODTCTRL register seems to have ODT disabled for READ accesses since the lower 4 bits are set to "7"? I have read all of the ODT threads here and there seems to be a lot confusion about setting ODT properly. I have used Hyperlynx on iMX31 and&lt;/P&gt;&lt;P&gt;iMX53 designs before and have had excellent correlation to the physical design. I want to make sure I translate the simulation output into correct register settings in the initialization code. My design emulates the Sabre SD board but&lt;/P&gt;&lt;P&gt;was laid out in Expedition instead or Cadence allegro. Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 18:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ODT-setting/m-p/462734#M72745</guid>
      <dc:creator>sparkyee</dc:creator>
      <dc:date>2016-05-11T18:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: ODT setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ODT-setting/m-p/462735#M72746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ODT settings of IOMUX are for the DDR Address and control pins, &lt;/P&gt;&lt;P&gt;and the ODT settings of MMDCx_MPODTCTRL are for the Data bus (by byte group).&lt;/P&gt;&lt;P&gt;So you can controls the ODT value for each byte group by the ODTx_INT_RES.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 00:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ODT-setting/m-p/462735#M72746</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-12T00:26:11Z</dc:date>
    </item>
  </channel>
</rss>