<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Build BSP with crosstool-NG in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Build-BSP-with-crosstool-NG/m-p/462718#M72741</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build the meta-fsl-bsp-release using a specific toolchain&lt;/P&gt;&lt;P&gt;I have installed (but not configured) crosstool-ng&lt;/P&gt;&lt;P&gt;I have 2 questions:&lt;/P&gt;&lt;P&gt;1) what do I configure ct-ng to be ?&lt;/P&gt;&lt;P&gt;arm-cortex_a8-linux-gnueabi&lt;/P&gt;&lt;P&gt;arm-unknown-linux-gnueabi&lt;/P&gt;&lt;P&gt;The built in cross compiler looks like cortexa9hf-vfp-neon-poky-linux-gnueabi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) How do I tell Yocto to use my toolchain ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Mar 2016 22:06:59 GMT</pubDate>
    <dc:creator>johnlaughton</dc:creator>
    <dc:date>2016-03-09T22:06:59Z</dc:date>
    <item>
      <title>Build BSP with crosstool-NG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-BSP-with-crosstool-NG/m-p/462718#M72741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build the meta-fsl-bsp-release using a specific toolchain&lt;/P&gt;&lt;P&gt;I have installed (but not configured) crosstool-ng&lt;/P&gt;&lt;P&gt;I have 2 questions:&lt;/P&gt;&lt;P&gt;1) what do I configure ct-ng to be ?&lt;/P&gt;&lt;P&gt;arm-cortex_a8-linux-gnueabi&lt;/P&gt;&lt;P&gt;arm-unknown-linux-gnueabi&lt;/P&gt;&lt;P&gt;The built in cross compiler looks like cortexa9hf-vfp-neon-poky-linux-gnueabi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) How do I tell Yocto to use my toolchain ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 22:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-BSP-with-crosstool-NG/m-p/462718#M72741</guid>
      <dc:creator>johnlaughton</dc:creator>
      <dc:date>2016-03-09T22:06:59Z</dc:date>
    </item>
    <item>
      <title>Re: Build BSP with crosstool-NG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-BSP-with-crosstool-NG/m-p/462719#M72742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello John Laughton,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You didn’t mention which processor you are using and I haven’t personally tested it but I would go with arm-unknown-linux-gnueabi unless you are indeed seeking to build a toolchain for a CortexA8. The BSP supports the i.MX6 which is a CortexA9 processor and hence cortexa9hf-vfp-neon-poky-linux-gnueabi is used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for how to force Yocto to use an external toolchain, please see section 3.5 of the Yocto Project Application Developer’s Guide (link below)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/latest/adt-manual/adt-manual.html#optionally-using-an-external-toolchain"&gt;http://www.yoctoproject.org/docs/latest/adt-manual/adt-manual.html#optionally-using-an-external-toolchain&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 17:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-BSP-with-crosstool-NG/m-p/462719#M72742</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-03-11T17:32:23Z</dc:date>
    </item>
  </channel>
</rss>