<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LTIB error - could not glob rpm in line 2410 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462323#M72648</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check if environment setup is correct, as recommended&lt;/P&gt;&lt;P&gt;for LTIB. Please refer to the enclosed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jan 2016 05:03:10 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-01-05T05:03:10Z</dc:date>
    <item>
      <title>LTIB error - could not glob rpm in line 2410</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462322#M72647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to install LTIB from L2.6.35_11.09.01_ER_source_bundle.tar.gz for i.mx53 under Ubunto 14.04 64 bit.&lt;/P&gt;&lt;P&gt;the build fails and I get the following error:&lt;/P&gt;&lt;P&gt;--------------------------&lt;/P&gt;&lt;P&gt;checking whether the C compiler (/home/haim/Downloads/gcc-linaro-5.2-2015.11-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-&amp;nbsp; ) works... no&lt;/P&gt;&lt;P&gt;configure: error: installation or configuration problem: C compiler cannot create executables.&lt;/P&gt;&lt;P&gt;error: Bad exit status from /home/haim/imx53-sw/ltib/tmp/rpm-tmp.UZAHzv (%build)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RPM build errors:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bad exit status from /home/haim/imx53-sw/ltib/tmp/rpm-tmp.UZAHzv (%build)&lt;/P&gt;&lt;P&gt;Build time for rpm-fs: 2 seconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Failed building rpm-fs&lt;/P&gt;&lt;P&gt;could not glob rpm in: /tmp/rpm-haim/RPMS/x86_64/rpm-fs-* at ./ltib line 2410.&lt;/P&gt;&lt;P&gt;traceback:&lt;/P&gt;&lt;P&gt; main::check_rpm_setup:2410&lt;/P&gt;&lt;P&gt;&amp;nbsp; main::host_checks:1423&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; main:542&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Started: Sun Jan&amp;nbsp; 3 12:12:21 2016&lt;/P&gt;&lt;P&gt;Ended:&amp;nbsp;&amp;nbsp; Sun Jan&amp;nbsp; 3 12:12:24 2016&lt;/P&gt;&lt;P&gt;Elapsed: 3 seconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These packages failed to build:&lt;/P&gt;&lt;P&gt;rpm-fs &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build Failed&lt;/P&gt;&lt;P&gt;---------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any thoughts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 10:55:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462322#M72647</guid>
      <dc:creator>hjdd</dc:creator>
      <dc:date>2016-01-03T10:55:20Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB error - could not glob rpm in line 2410</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462323#M72648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check if environment setup is correct, as recommended&lt;/P&gt;&lt;P&gt;for LTIB. Please refer to the enclosed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 05:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462323#M72648</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-01-05T05:03:10Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB error - could not glob rpm in line 2410</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462324#M72649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the pdf you enclosed was written for ubuntu 9.04.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is is still valid to ubuntu 14.04? are there any patches needed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 10:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-error-could-not-glob-rpm-in-line-2410/m-p/462324#M72649</guid>
      <dc:creator>hjdd</dc:creator>
      <dc:date>2016-01-06T10:56:33Z</dc:date>
    </item>
  </channel>
</rss>