<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCompatibility of i.Mx6Q processor with Redpine wifi module RS9113 for SDIO interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-of-i-Mx6Q-processor-with-Redpine-wifi-module/m-p/461133#M72402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I;m using i.Mx6Q in my design with Wifi module RS9113-N00-D0N. &lt;/P&gt;&lt;P&gt;I want to interface these with SDIO signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the Datasheets the RS9113 has SDIO 2.0 interface, and i.Mx6Q has SDIO 3.0 interface (SDIO1 will be used).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, are the two parts are compatible with each other ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the SDIO 3.0 of i.Mx6 is backword compatible with SDIO 2.0 of RS9113 wifi module ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply ASAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Nanjunda M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jan 2016 07:22:15 GMT</pubDate>
    <dc:creator>nanjundam</dc:creator>
    <dc:date>2016-01-25T07:22:15Z</dc:date>
    <item>
      <title>Compatibility of i.Mx6Q processor with Redpine wifi module RS9113 for SDIO interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-of-i-Mx6Q-processor-with-Redpine-wifi-module/m-p/461133#M72402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I;m using i.Mx6Q in my design with Wifi module RS9113-N00-D0N. &lt;/P&gt;&lt;P&gt;I want to interface these with SDIO signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the Datasheets the RS9113 has SDIO 2.0 interface, and i.Mx6Q has SDIO 3.0 interface (SDIO1 will be used).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, are the two parts are compatible with each other ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the SDIO 3.0 of i.Mx6 is backword compatible with SDIO 2.0 of RS9113 wifi module ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply ASAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Nanjunda M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 07:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-of-i-Mx6Q-processor-with-Redpine-wifi-module/m-p/461133#M72402</guid>
      <dc:creator>nanjundam</dc:creator>
      <dc:date>2016-01-25T07:22:15Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of i.Mx6Q processor with Redpine wifi module RS9113 for SDIO interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-of-i-Mx6Q-processor-with-Redpine-wifi-module/m-p/461134#M72403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nanjunda&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes i.MX6 SDIO 3.0 is backward compatible with SDIO 2.0, RS9113 wifi module&lt;/P&gt;&lt;P&gt;can be used with i.MX6 processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 07:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-of-i-Mx6Q-processor-with-Redpine-wifi-module/m-p/461134#M72403</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-25T07:41:23Z</dc:date>
    </item>
  </channel>
</rss>