<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power up problems VDDIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460735#M72321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We actually use  the SPI master SSP2 boot from Flash 3.3V and the LCD_RS is set to 1.&lt;/P&gt;&lt;P&gt;D6-D0: 0 0 0 0 0 1 0&lt;/P&gt;&lt;P&gt;I test your proposal and the behaviour is the same:&lt;/P&gt;&lt;P&gt;The DCDC_VDDIO drops from 3.3V to 2.6V after the release of the RESET_N.&lt;/P&gt;&lt;P&gt;I guess there is a wrong setting of a bit or value in the HW_POWER memory map.&lt;/P&gt;&lt;P&gt;Some trials from my side are not successful till now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mit freundlichen Gruessen / Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin Steurer&lt;/P&gt;&lt;P&gt;AES Aerospace Embedded Solutions GmbH&lt;/P&gt;&lt;P&gt;Abteilungsbezeichnung TEE&lt;/P&gt;&lt;P&gt;Department TEE&lt;/P&gt;&lt;P&gt;Friedenheimer Brücke 29&lt;/P&gt;&lt;P&gt;80639 Muenchen&lt;/P&gt;&lt;P&gt;Germany&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tel +49 (0)89 99 82 72-32 01&lt;/P&gt;&lt;P&gt;Fax +49 (0)89 99 82 72-71 072&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mailto:martin.steurer@aesolutions.de&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.aesolutions.de&amp;lt;http://www.aesolutions.de/&amp;gt;" target="test_blank"&gt;http://www.aesolutions.de&amp;lt;http://www.aesolutions.de/&amp;gt;&lt;/A&gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: igorpadykov &lt;/P&gt;&lt;P&gt;Gesendet: Mittwoch, 9. März 2016 02:27&lt;/P&gt;&lt;P&gt;An: STEURER, Martin &amp;lt;Martin.Steurer@aesolutions.de&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Power up problems VDDIO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Power up problems VDDIO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from igorpadykov&amp;lt;https://community.freescale.com/people/igorpadykov?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/622737?et=watches.email.thread#comment-622737&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Mar 2016 08:38:42 GMT</pubDate>
    <dc:creator>martinsteurer</dc:creator>
    <dc:date>2016-03-09T08:38:42Z</dc:date>
    <item>
      <title>Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460732#M72318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;there are problems during power up with the internal generated voltage VDDIO.&lt;/P&gt;&lt;P&gt;The circuit on my target is similar to the Eval-Board and there is the possibility to power the device by 5V via VDD5V or with 3.3V generated by a flyback via Battery/DCDC_Batt.&lt;/P&gt;&lt;P&gt;The target is connected to a Lauterbach. If the target is powered by 5V I had access to the controller independent if the IMX287 is held in reset or not.&lt;/P&gt;&lt;P&gt;If the target is powered with the 3.3V I have only access to the target in reset condition. By release the reset, the VDDIO voltage drop to 2.5V and there is no communication possible with the Lauterbach.&lt;/P&gt;&lt;P&gt;Different settings of the Registers HW_POWER_5VCTRL, HW_POWER_VDDIOCTRL and HW_POWER_DCDC4P2 are till now not successful.&lt;/P&gt;&lt;P&gt;Is there a special setting necessary or what could be the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 12:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460732#M72318</guid>
      <dc:creator>martinsteurer</dc:creator>
      <dc:date>2016-03-08T12:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460733#M72319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is "Wait JTAG connection mode" described in &lt;/P&gt;&lt;P&gt;Table 12-3. Boot Mode Selection Map&amp;nbsp; i.MX28 Reference Manual &lt;/P&gt;&lt;P&gt;could you try it.&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2Fdsp%2Fdoc%2Fref_manual%2FMCIMX28RM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 01:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460733#M72319</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-09T01:25:46Z</dc:date>
    </item>
    <item>
      <title>Re: Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460734#M72320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we actually use&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 8pt;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 8pt;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 8pt;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;0 0 0 0 0 1 0 SPI2 SPI master SSP2 boot from flash, 3.3 V (LCD_RS 1)&lt;/P&gt;&lt;P&gt;I could try the ,Wait JTAG connection mode'...&lt;/P&gt;&lt;P&gt;Test finished.&lt;/P&gt;&lt;P&gt;With this Boot Mode the behavior is the same! Independent if the Lauterbach is connected or not.&lt;/P&gt;&lt;P&gt;The DCDC_VDDIO drops from 3.3V to 2.6V after the release of the RESET_N.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 8pt;"&gt;&lt;SPAN lang="JA" style="font-family: HelveticaLTStd-Roman; font-size: 8pt;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 08:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460734#M72320</guid>
      <dc:creator>martinsteurer</dc:creator>
      <dc:date>2016-03-09T08:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460735#M72321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We actually use  the SPI master SSP2 boot from Flash 3.3V and the LCD_RS is set to 1.&lt;/P&gt;&lt;P&gt;D6-D0: 0 0 0 0 0 1 0&lt;/P&gt;&lt;P&gt;I test your proposal and the behaviour is the same:&lt;/P&gt;&lt;P&gt;The DCDC_VDDIO drops from 3.3V to 2.6V after the release of the RESET_N.&lt;/P&gt;&lt;P&gt;I guess there is a wrong setting of a bit or value in the HW_POWER memory map.&lt;/P&gt;&lt;P&gt;Some trials from my side are not successful till now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mit freundlichen Gruessen / Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin Steurer&lt;/P&gt;&lt;P&gt;AES Aerospace Embedded Solutions GmbH&lt;/P&gt;&lt;P&gt;Abteilungsbezeichnung TEE&lt;/P&gt;&lt;P&gt;Department TEE&lt;/P&gt;&lt;P&gt;Friedenheimer Brücke 29&lt;/P&gt;&lt;P&gt;80639 Muenchen&lt;/P&gt;&lt;P&gt;Germany&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tel +49 (0)89 99 82 72-32 01&lt;/P&gt;&lt;P&gt;Fax +49 (0)89 99 82 72-71 072&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mailto:martin.steurer@aesolutions.de&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.aesolutions.de&amp;lt;http://www.aesolutions.de/&amp;gt;" target="test_blank"&gt;http://www.aesolutions.de&amp;lt;http://www.aesolutions.de/&amp;gt;&lt;/A&gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: igorpadykov &lt;/P&gt;&lt;P&gt;Gesendet: Mittwoch, 9. März 2016 02:27&lt;/P&gt;&lt;P&gt;An: STEURER, Martin &amp;lt;Martin.Steurer@aesolutions.de&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Power up problems VDDIO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Power up problems VDDIO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from igorpadykov&amp;lt;https://community.freescale.com/people/igorpadykov?et=watches.email.thread&amp;gt; in i.MX Community - View the full discussion&amp;lt;https://community.freescale.com/message/622737?et=watches.email.thread#comment-622737&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 08:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460735#M72321</guid>
      <dc:creator>martinsteurer</dc:creator>
      <dc:date>2016-03-09T08:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460736#M72322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if VDDIO is affected by brownout: tweak BO_OFFSET&lt;/P&gt;&lt;P&gt;in VDDIOCTRL. Could VDDIO be overloaded ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 10:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460736#M72322</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-09T10:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: Power up problems VDDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460737#M72323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Calibri',sans-serif; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-language: EN-US;"&gt;We step through the initialization and found the wrong setting in the power register&lt;BR /&gt;HW_POWER_5VCTRL and HW_POWER_VDDACTRL.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Calibri',sans-serif; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-language: EN-US;"&gt;Now it works. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Calibri',sans-serif; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-language: EN-US;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="color: #1f497d; font-family: 'Calibri',sans-serif; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-language: EN-US;"&gt;Thanks for your help&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 05:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-up-problems-VDDIO/m-p/460737#M72323</guid>
      <dc:creator>martinsteurer</dc:creator>
      <dc:date>2016-03-11T05:50:59Z</dc:date>
    </item>
  </channel>
</rss>