<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Display resolution messed up when switching to console</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460669#M72294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there anybody out there who knows what I should do to fix this behaviour?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 May 2016 08:35:17 GMT</pubDate>
    <dc:creator>hiromiyokoo</dc:creator>
    <dc:date>2016-05-16T08:35:17Z</dc:date>
    <item>
      <title>Display resolution messed up when switching to console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460668#M72293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a board with an iMX6DL with a yocto poky qt-in-use-image distro.&lt;/P&gt;&lt;P&gt;I'm not launching the default application, instead I'm using a qt example this way:&lt;/P&gt;&lt;P&gt;export DISPLAY=:0&lt;/P&gt;&lt;P&gt;cd ~/declarative/animation/basics/color-animation&lt;/P&gt;&lt;P&gt;Xorg &amp;amp;&lt;/P&gt;&lt;P&gt;./color-animation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works like a charm, but when I try to switch to a console with &amp;lt;ctrl&amp;gt;&amp;lt;alt&amp;gt;&amp;lt;f1&amp;gt; and then go back to X with &amp;lt;ctrl&amp;gt;&amp;lt;alt&amp;gt;&amp;lt;f2&amp;gt; (or &amp;lt;f3&amp;gt; sometimes), the image on the LVDS display is all messed up. It's composed of black and white lines (no colour signals). The application is still responding (I can see in some way the image, messed up) and I can move the mouse pointer.&lt;/P&gt;&lt;P&gt;The same issue happens when I try to suspend with:&lt;/P&gt;&lt;P&gt;echo mem &amp;gt; /sys/power/state&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;echo standby &amp;gt; /sys/power/state&lt;/P&gt;&lt;P&gt;and then resume with the power button. The image becomes a mess.&lt;/P&gt;&lt;P&gt;If I kill Xorg and the qt example, and launch them again, I get a perfect image again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the log /var/volatile/log/Xorg.0.log the weird outputs are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[2673309.221] (**) Option "config_info" "udev:/sys/devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.4/1-1.4.3/1-1.4.3:1.0/input/input2/event2"&lt;/P&gt;&lt;P&gt;[2673309.221] (II) XINPUT: Adding extended input device "Lite-On Technology Corp. HP Basic USB Keyboard" (type: KEYBOARD, id 8)&lt;/P&gt;&lt;P&gt;[2673309.221] (**) Option "xkb_rules" "evdev"&lt;/P&gt;&lt;P&gt;[2673309.221] (**) Option "xkb_model" "pc104"&lt;/P&gt;&lt;P&gt;[2673309.221] (**) Option "xkb_layout" "us"&lt;/P&gt;&lt;P&gt;[2673392.361] &lt;STRONG&gt;setversion 1.4 failed&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;[2673744.380] (II) evdev: Lite-On Technology Corp. HP Basic USB Keyboard: Close&lt;/P&gt;&lt;P&gt;[2673744.380] (II) UnloadModule: "evdev"&lt;/P&gt;&lt;P&gt;[2673744.381] (II) evdev: USB Optical Mouse: Close&lt;/P&gt;&lt;P&gt;[2673744.381] (II) UnloadModule: "evdev"&lt;/P&gt;&lt;P&gt;[2673744.381] (II) evdev: 20b8000.kpp: Close&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[2673308.891] drmOpenDevice: node name is /dev/dri/card0&lt;/P&gt;&lt;P&gt;[2673308.891] drmOpenDevice: open result is 13, (OK)&lt;/P&gt;&lt;P&gt;[2673308.891] drmOpenByBusid: drmOpenMinor returns 13&lt;/P&gt;&lt;P&gt;[2673308.891] drmOpenByBusid: Interface 1.4 failed, trying 1.1&lt;/P&gt;&lt;P&gt;[2673308.891] drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore:00&lt;/P&gt;&lt;P&gt;[2673308.894] &lt;STRONG&gt;(EE) AIGLX error&lt;/STRONG&gt;: vivante exports no extensions (/usr/lib/dri/vivante_dri.so: undefined symbol: __driDriverExtensions)&lt;/P&gt;&lt;P&gt;[2673308.894] (EE) AIGLX: reverting to software rendering&lt;/P&gt;&lt;P&gt;[2673308.917] (II) AIGLX: Loaded and initialized swrast&lt;/P&gt;&lt;P&gt;[2673308.918] (II) GLX: Initialized DRISWRAST GL provider for screen 0&lt;/P&gt;&lt;P&gt;[2673308.921] (II) &lt;STRONG&gt;VIVANTE(0): Setting screen physical size to 211 x 127&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;[2673309.082] (II) config/udev: Adding drm device (/dev/dri/card0)&lt;/P&gt;&lt;P&gt;[2673309.084] (II) config/udev: Adding input device 20b8000.kpp (/dev/input/event0)&lt;/P&gt;&lt;P&gt;[2673309.084] (**) 20b8000.kpp: Applying InputClass "evdev keyboard catchall"&lt;/P&gt;&lt;P&gt;[2673309.084] (II) LoadModule: "evdev"&lt;/P&gt;&lt;P&gt;[2673309.084] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 11:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460668#M72293</guid>
      <dc:creator>hiromiyokoo</dc:creator>
      <dc:date>2016-05-11T11:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: Display resolution messed up when switching to console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460669#M72294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there anybody out there who knows what I should do to fix this behaviour?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2016 08:35:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460669#M72294</guid>
      <dc:creator>hiromiyokoo</dc:creator>
      <dc:date>2016-05-16T08:35:17Z</dc:date>
    </item>
    <item>
      <title>Re: Display resolution messed up when switching to console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460670#M72295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to send SIGUSR1 to X server for it to re-init the display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 May 2016 07:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460670#M72295</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-05-20T07:00:51Z</dc:date>
    </item>
    <item>
      <title>Re: Display resolution messed up when switching to console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460671#M72296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help, I tried to put my application into the startx script and now it works perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 May 2016 09:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-resolution-messed-up-when-switching-to-console/m-p/460671#M72296</guid>
      <dc:creator>hiromiyokoo</dc:creator>
      <dc:date>2016-05-24T09:52:58Z</dc:date>
    </item>
  </channel>
</rss>