<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Probing a device connected on sdio lines? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460616#M72271</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to your reply, Actually I'm writing a generic code(application) that detect device connected which mainly bit 1/4 mode. for that i need a way to write a code how and where to start. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Mar 2016 07:35:40 GMT</pubDate>
    <dc:creator>gbiradar</dc:creator>
    <dc:date>2016-03-08T07:35:40Z</dc:date>
    <item>
      <title>Probing a device connected on sdio lines?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460614#M72269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm trying to write a simple application for imx6 board whose job is to read the information of device/module connected via sdio lines, the device can be 1 bit, 4 bit or spi also and the device/module&amp;nbsp; can be anything sd card, wireless etc...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know where to start i have downloaded standard specification sdio, but application side how do i start because as per my knowledge sdio doesn't have any node in /dev/....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if anyone has to probe the device basic idea how can we probe. this application should probe device id or vendor id in short status/category of the device connected on sdio lines.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Ganesh Biradar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 06:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460614#M72269</guid>
      <dc:creator>gbiradar</dc:creator>
      <dc:date>2016-03-08T06:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: Probing a device connected on sdio lines?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460615#M72270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ganesh,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For your questions, I can just give you some sugggestions !&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(1) Don't suggest you use uSDHC interface&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;If you use the interface, your device should support SDIO / SD / eMMC protocol.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(2) SPI interface recommended&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;If you connect your device to SPI port of i.MX6, you can use "spidev" driver in linux BSP, the way can help you save development time. As for how to use spidev, you can get more information from internet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hope above adivce can help you !&lt;/P&gt;&lt;P&gt;Good luck!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 07:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460615#M72270</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-03-08T07:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: Probing a device connected on sdio lines?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460616#M72271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to your reply, Actually I'm writing a generic code(application) that detect device connected which mainly bit 1/4 mode. for that i need a way to write a code how and where to start. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 07:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460616#M72271</guid>
      <dc:creator>gbiradar</dc:creator>
      <dc:date>2016-03-08T07:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: Probing a device connected on sdio lines?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460617#M72272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ganesh,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Anyway, you need to write a driver for your device at first, and in your driver, you should provide function interface for linux application. Otherwise, we can't access the device from linux application.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 08:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460617#M72272</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-03-08T08:19:40Z</dc:date>
    </item>
    <item>
      <title>Re: Probing a device connected on sdio lines?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460618#M72273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;                   My self i am VIjay. I am developing a custom board with&lt;/P&gt;&lt;P&gt;reference of sabresd but i am facing below problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. EDID for HDMI is not working properly even i config with i2c properly.It&lt;/P&gt;&lt;P&gt;showing below message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: No modes read from edid&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: create default modelist&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: Read EDID again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: No modes read from edid&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: create default modelist&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Actually i want to connect with the board 1280x768 @ 65Hz but it always&lt;/P&gt;&lt;P&gt;config to 640x480@60Hz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp; I seen the EDID supportable parameters under&lt;/P&gt;&lt;P&gt;/driver/video/mxc/mxc_edid.c(also configured to 1280x720 @ 60Hz ) like&lt;/P&gt;&lt;P&gt;below. but display not working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 17:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Probing-a-device-connected-on-sdio-lines/m-p/460618#M72273</guid>
      <dc:creator>vijay_jay5</dc:creator>
      <dc:date>2016-03-09T17:36:20Z</dc:date>
    </item>
  </channel>
</rss>