<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSGTL5000 problems on iMX53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178742#M7226</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, my board is based on the imx53 QSB and uses the SGTL5000 sound chip connected up in the same way. &amp;nbsp;When the kernel loads I get this error:-&lt;/P&gt;&lt;P&gt;sgtl5000_hw_read: read reg error : Reg 0x00 &lt;BR /&gt;Device with ID register 0 is not a SGTL5000 &lt;BR /&gt;No device for DAI imx-ssi-1-0 &lt;BR /&gt;No device for DAI imx-ssi-1-1 &lt;BR /&gt;No device for DAI imx-ssi-2-0 &lt;BR /&gt;No device for DAI imx-ssi-2-1 &lt;BR /&gt;ALSA device list: &lt;BR /&gt; No soundcards found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So no sound!&lt;/P&gt;&lt;P&gt;I tried to add in SSI in the kernel config, but the build.&lt;/P&gt;&lt;P&gt;Can anyone tell me if I need SSI for SGTL5000 support?&lt;/P&gt;&lt;P&gt;If so, what is it dependent on? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I noticed that if I read back&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_KEY_COL3 and&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_KEY_ROW3 after boot, they are both set to 0x00000014 which is software override mode (SION), not the ALT4 mode which I need. &amp;nbsp;I'm setting it in u-boot but it's getting overwritten by something in the kernel - I don't know what! &amp;nbsp;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jul 2012 15:31:07 GMT</pubDate>
    <dc:creator>NeilSimpson</dc:creator>
    <dc:date>2012-07-31T15:31:07Z</dc:date>
    <item>
      <title>SGTL5000 problems on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178742#M7226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, my board is based on the imx53 QSB and uses the SGTL5000 sound chip connected up in the same way. &amp;nbsp;When the kernel loads I get this error:-&lt;/P&gt;&lt;P&gt;sgtl5000_hw_read: read reg error : Reg 0x00 &lt;BR /&gt;Device with ID register 0 is not a SGTL5000 &lt;BR /&gt;No device for DAI imx-ssi-1-0 &lt;BR /&gt;No device for DAI imx-ssi-1-1 &lt;BR /&gt;No device for DAI imx-ssi-2-0 &lt;BR /&gt;No device for DAI imx-ssi-2-1 &lt;BR /&gt;ALSA device list: &lt;BR /&gt; No soundcards found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So no sound!&lt;/P&gt;&lt;P&gt;I tried to add in SSI in the kernel config, but the build.&lt;/P&gt;&lt;P&gt;Can anyone tell me if I need SSI for SGTL5000 support?&lt;/P&gt;&lt;P&gt;If so, what is it dependent on? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I noticed that if I read back&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_KEY_COL3 and&amp;nbsp;IOMUXC_SW_MUX_CTL_PAD_KEY_ROW3 after boot, they are both set to 0x00000014 which is software override mode (SION), not the ALT4 mode which I need. &amp;nbsp;I'm setting it in u-boot but it's getting overwritten by something in the kernel - I don't know what! &amp;nbsp;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2012 15:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178742#M7226</guid>
      <dc:creator>NeilSimpson</dc:creator>
      <dc:date>2012-07-31T15:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 problems on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178743#M7227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fixed!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2012 11:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178743#M7227</guid>
      <dc:creator>NeilSimpson</dc:creator>
      <dc:date>2012-08-03T11:09:15Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 problems on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178744#M7228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've just boot QSB coming with ubuntu out of the box:&lt;/P&gt;&lt;P&gt;lucid-desktop login: lucid&lt;BR /&gt;Password: &lt;BR /&gt;sgtl5000_hw_read: read reg error : Reg 0x0e&lt;BR /&gt;sgtl5000_write: write reg error : Reg 0x0e = 0x000c&lt;BR /&gt;sgtl5000_write: write reg error : Reg 0x02 = 0x0020&lt;BR /&gt;Last login: Thu Jan&amp;nbsp; 1 08:04:40 CST 1970 on ttymxc0&lt;BR /&gt;sgtl5000_write: write reg error : Reg 0x06 = 0x0130&lt;BR /&gt;Linux lucid-desktop 2.6.35.3-1129-g691c08a #7 PREEMPT Wed Nov 16 14:33:06 BRST 2011 armv7l GNU/Linux&lt;BR /&gt;Ubuntu 10.04 LTS&lt;BR /&gt;&lt;BR /&gt;Welcome to Ubuntu!&lt;BR /&gt;&amp;nbsp;* Documentation:&amp;nbsp; &lt;A href="https://help.ubuntu.com/" target="_blank"&gt;https://help.ubuntu.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~`&lt;BR /&gt;It's just warnings?&lt;BR /&gt;because the video demo works with sound, but when trying Gstreamer, only video works without audio.&lt;/P&gt;&lt;P&gt;&amp;nbsp; gst-launch udpsrc port=5656 caps="application/x-rtp, media=audio, clock-rate=8000, encoding-name=PCMU, payload=0, ssrc=1253488865, clock-base=3079727525, seqnum-base=32302" ! queue ! rtppcmudepay ! mulawdec ! audioconvert ! alsasink -v&lt;/P&gt;&lt;P&gt;TNX,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2012 20:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178744#M7228</guid>
      <dc:creator>ChaimA</dc:creator>
      <dc:date>2012-08-20T20:24:22Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 problems on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178745#M7229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I'm having the same issue. What have you done to fix it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2012 18:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178745#M7229</guid>
      <dc:creator>RafaelThomasGoz</dc:creator>
      <dc:date>2012-10-30T18:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: SGTL5000 problems on iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178746#M7230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got it fixed, the problem was actually a bad HW that was introducing noise on the I2C channel and breaking my BSP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2012 16:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SGTL5000-problems-on-iMX53/m-p/178746#M7230</guid>
      <dc:creator>RafaelThomasGoz</dc:creator>
      <dc:date>2012-11-16T16:00:08Z</dc:date>
    </item>
  </channel>
</rss>