<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using Camera without I2C in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-Camera-without-I2C/m-p/460520#M72252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a Nitrogen6q (i.mx6 quad) board with Ubuntu (or Yocto) running and want to connect a camera to it. This camera has no I2C bus Connection. Now i am wondering how the camera could be recognized by&amp;nbsp; the OS and with what kind of software the Images can be handled. The camera is connectet to the parallel camera port with a 17-bit interface (14bit Pixel data + pixel_clk + line/frame_valid) and can be configured via RS-232.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Dec 2015 14:26:39 GMT</pubDate>
    <dc:creator>patrickwiegand</dc:creator>
    <dc:date>2015-12-03T14:26:39Z</dc:date>
    <item>
      <title>Using Camera without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Camera-without-I2C/m-p/460520#M72252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a Nitrogen6q (i.mx6 quad) board with Ubuntu (or Yocto) running and want to connect a camera to it. This camera has no I2C bus Connection. Now i am wondering how the camera could be recognized by&amp;nbsp; the OS and with what kind of software the Images can be handled. The camera is connectet to the parallel camera port with a 17-bit interface (14bit Pixel data + pixel_clk + line/frame_valid) and can be configured via RS-232.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 14:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Camera-without-I2C/m-p/460520#M72252</guid>
      <dc:creator>patrickwiegand</dc:creator>
      <dc:date>2015-12-03T14:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: Using Camera without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-Camera-without-I2C/m-p/460521#M72253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;new camera integration steps are quite well described in&lt;/P&gt;&lt;P&gt;i.MX53 System Development User’s Guide (rev.1, 3/2011)&lt;/P&gt;&lt;P&gt;Chapter 19 Supporting the i.MX53 Camera Sensor Interface CSI0,&lt;/P&gt;&lt;P&gt;though for older kernel. One can try to change i2c control channel to uart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf" rel="nofollow"&gt;http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For i.MX6 IPU connections and supported formats one can look at&lt;/P&gt;&lt;P&gt;Table 66. Camera Input Signal Cross Reference, Format, and Bits Per Cycle&lt;/P&gt;&lt;P&gt;i.MX6DQ Datasheet (rev.4, 7/2015)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 01:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-Camera-without-I2C/m-p/460521#M72253</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-04T01:31:25Z</dc:date>
    </item>
  </channel>
</rss>