<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Display chinese characters in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-chinese-characters/m-p/459897#M72114</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I work on imx6 quad based custom board which runs Yocto based linux 3.10.17 kernel. I have some chinese mp3 songs on USB. When i mount USB drive and try ls command&lt;/P&gt;&lt;P&gt;It shows question marks instead of chinese characters in the mp3 filenames,&lt;/P&gt;&lt;P&gt;Do we need to set any kernel config/ busybox config ? or environment variable?&lt;/P&gt;&lt;P&gt;I already have UTF8 NLS config enabled in kernel.&lt;/P&gt;&lt;P&gt;Also do we need to add some package in rootfs for the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Dec 2015 09:30:10 GMT</pubDate>
    <dc:creator>sharvari</dc:creator>
    <dc:date>2015-12-31T09:30:10Z</dc:date>
    <item>
      <title>Display chinese characters</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-chinese-characters/m-p/459897#M72114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I work on imx6 quad based custom board which runs Yocto based linux 3.10.17 kernel. I have some chinese mp3 songs on USB. When i mount USB drive and try ls command&lt;/P&gt;&lt;P&gt;It shows question marks instead of chinese characters in the mp3 filenames,&lt;/P&gt;&lt;P&gt;Do we need to set any kernel config/ busybox config ? or environment variable?&lt;/P&gt;&lt;P&gt;I already have UTF8 NLS config enabled in kernel.&lt;/P&gt;&lt;P&gt;Also do we need to add some package in rootfs for the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 09:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-chinese-characters/m-p/459897#M72114</guid>
      <dc:creator>sharvari</dc:creator>
      <dc:date>2015-12-31T09:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: Display chinese characters</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-chinese-characters/m-p/459898#M72115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This migth help&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/563420"&gt;https://community.nxp.com/message/563420&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 15:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-chinese-characters/m-p/459898#M72115</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-09-28T15:39:27Z</dc:date>
    </item>
  </channel>
</rss>