<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using i.MX as a Media Center, Audio Stream with S/PDIF in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459754#M72081</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atilla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this setup is enough to make it work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jan 2016 08:17:29 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-01-04T08:17:29Z</dc:date>
    <item>
      <title>Using i.MX as a Media Center, Audio Stream with S/PDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459751#M72078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a multimedia centre using the imx6 and new to most of the stuff I come across with.&lt;/P&gt;&lt;P&gt;As part of the design I would like the card to support 5.1 and 7.1 home theater systems and for this&lt;/P&gt;&lt;P&gt;purpose, planning to use the S/PDIF interface that imx6 has.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simply put my question is what intermediate ICs and devices do I need to connect in between my&lt;/P&gt;&lt;P&gt;home theather system and imx6 in case of;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Coaxial&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Optical (TOSLINK)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I give outputs from the Tx of the S/PDIF, how do I convert it to optical? If I use a coaxial connector&lt;/P&gt;&lt;P&gt;do I need nothing else but the cable in between? Obviously home theathre handles the DAC if it accepts&lt;/P&gt;&lt;P&gt;S/PDIF so that is not my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A detailed explanation or guidance is welcome since I am completely new and self educated on the subject.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 11:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459751#M72078</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2015-12-30T11:59:12Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX as a Media Center, Audio Stream with S/PDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459752#M72079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atilla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for convertion to optical one can use for example&lt;/P&gt;&lt;P&gt;GP1FAV30RK0F,GP1FMV31TK0F. Common description&lt;/P&gt;&lt;P&gt;can be found on:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://en.wikipedia.org/wiki/S/PDIF" rel="nofollow"&gt;https://en.wikipedia.org/wiki/S/PDIF&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://en.wikipedia.org/wiki/TOSLINK" title="https://en.wikipedia.org/wiki/TOSLINK"&gt;TOSLINK - Wikipedia, the free encyclopedia&lt;/A&gt; &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Jan 2016 06:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459752#M72079</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-02T06:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX as a Media Center, Audio Stream with S/PDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459753#M72080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. Just to make sure, please verify what I have in my mind.&lt;/P&gt;&lt;P&gt;Linux running on I.MX6&amp;nbsp; S/PDIF interface using a transmitter (&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;GP1FMV31TK0F&lt;/SPAN&gt;) connected&lt;/P&gt;&lt;P&gt;to a home theather system through an optical calbe (TOSLINK) will be a setup enough&lt;/P&gt;&lt;P&gt;to make it work (See attachment below for the Setup).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Atilla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMX6_SPDIF_Interface.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31557iEF52B17D4266F001/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMX6_SPDIF_Interface.jpg" alt="IMX6_SPDIF_Interface.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 06:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459753#M72080</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-01-04T06:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX as a Media Center, Audio Stream with S/PDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459754#M72081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atilla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this setup is enough to make it work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 08:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459754#M72081</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-04T08:17:29Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX as a Media Center, Audio Stream with S/PDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459755#M72082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Atilla&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 08:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX-as-a-Media-Center-Audio-Stream-with-S-PDIF/m-p/459755#M72082</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-01-04T08:19:43Z</dc:date>
    </item>
  </channel>
</rss>