<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 IPU: enqueue task with callback in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-enqueue-task-with-callback/m-p/459463#M72014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; According to Image Processing Unit (IPU) Drivers chapter in "i.MX_Linux_Reference_Manual.pdf",&lt;/P&gt;&lt;P&gt;for more information on what IOCTLs exist and which data structures they use, see&lt;/P&gt;&lt;P&gt;&amp;lt;Yocto_BuildDir&amp;gt;/linux/include/uapi/linux/fb.h.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Perhaps You need to implement the required feature yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jun 2016 08:20:52 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-06-10T08:20:52Z</dc:date>
    <item>
      <title>IMX6 IPU: enqueue task with callback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-enqueue-task-with-callback/m-p/459462#M72013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to enqueue a task to the IPU, I am currently using the following C function call in my program:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ioctl(fd_ipu, IPU_QUEUE_TASK, &amp;amp;task)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works, but it only returns when the enqueued task in the IPU is finished. I would like to do it in an non blocking way, by for example providing a callback function to the IPU, so that I can still use my thread during the ipu operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 18:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-enqueue-task-with-callback/m-p/459462#M72013</guid>
      <dc:creator>albanderuaz</dc:creator>
      <dc:date>2016-05-27T18:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 IPU: enqueue task with callback</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-enqueue-task-with-callback/m-p/459463#M72014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; According to Image Processing Unit (IPU) Drivers chapter in "i.MX_Linux_Reference_Manual.pdf",&lt;/P&gt;&lt;P&gt;for more information on what IOCTLs exist and which data structures they use, see&lt;/P&gt;&lt;P&gt;&amp;lt;Yocto_BuildDir&amp;gt;/linux/include/uapi/linux/fb.h.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Perhaps You need to implement the required feature yourself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 08:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-IPU-enqueue-task-with-callback/m-p/459463#M72014</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-10T08:20:52Z</dc:date>
    </item>
  </channel>
</rss>