<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Mfgtool Format Disc pop-up  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-Format-Disc-pop-up/m-p/458676#M71808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, this is not the MFGtool pop-up but the OS pop-up. It occurs at the moment when target board switches from emulating USB HID device to USB Mass-storage device. Typically, it occurs on slowly-running host OSes. Try to do it on a faster machine :-)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Sep 2015 08:47:03 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2015-09-22T08:47:03Z</dc:date>
    <item>
      <title>Mfgtool Format Disc pop-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-Format-Disc-pop-up/m-p/458675#M71807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;when we flash SW using Mfgtool "format disc popup" will appear (discarding&amp;nbsp; popup as it does not affect any functionality).&lt;/P&gt;&lt;P&gt;Is there any way we can fix in OS side to disable popup&amp;nbsp; as Mfgtool uses UTP protocol to transfer images i am not sure fixing that in OS side may have side effects &lt;/P&gt;&lt;P&gt;Is there any proven solution available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 04:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-Format-Disc-pop-up/m-p/458675#M71807</guid>
      <dc:creator>ashokkumarredd1</dc:creator>
      <dc:date>2015-09-18T04:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool Format Disc pop-up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-Format-Disc-pop-up/m-p/458676#M71808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, this is not the MFGtool pop-up but the OS pop-up. It occurs at the moment when target board switches from emulating USB HID device to USB Mass-storage device. Typically, it occurs on slowly-running host OSes. Try to do it on a faster machine :-)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 08:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool-Format-Disc-pop-up/m-p/458676#M71808</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-09-22T08:47:03Z</dc:date>
    </item>
  </channel>
</rss>