<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using TSC2007 touchscreen  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458379#M71731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;What the "126" at "clocks = &amp;lt;&amp;amp;clks 126&amp;gt;;" means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is IMX6QDL_CLK_I2C2 defined in&amp;nbsp; .../include/dt-bindings/clock/imx6qdl-clock.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Dec 2015 02:02:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-04T02:02:02Z</dc:date>
    <item>
      <title>Using TSC2007 touchscreen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458377#M71729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi every body!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're trying to use TSC2007 with i.MX6q, I've configured device-tree as following:&lt;/P&gt;&lt;P&gt;[code]&lt;/P&gt;&lt;P&gt;&amp;amp;i2c2 {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tsc2007: tsc2007@48 {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "ti,tsc2007";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x48&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt-parent = &amp;lt;&amp;amp;gpio3&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupts = &amp;lt;21 8&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; gpios = &amp;lt;&amp;amp;gpio3 21 0&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ti,x-plate-ohms = &amp;lt;400&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;[/code]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver is loading fine. I see the input device created at /dev/input/, when pressing the touch I can see the pointer moving in the screen but it doesn't click at all. I saw that no interrupt is triggered when the touch is pressed. Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also was looking for i2c current clock speed and find this at device tree:&lt;/P&gt;&lt;P&gt;[code]&lt;/P&gt;&lt;P&gt;i2c2: i2c@021a4000 {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #address-cells = &amp;lt;1&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #size-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x021a4000 0x4000&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupts = &amp;lt;0 37 0x04&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; clocks = &amp;lt;&amp;amp;clks 126&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "disabled";&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;[/code]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What the "126" at "clocks = &amp;lt;&amp;amp;clks 126&amp;gt;;" means? How can I determine the clock speed that i2c is using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;- dhs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 19:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458377#M71729</guid>
      <dc:creator>danielhilst</dc:creator>
      <dc:date>2015-12-03T19:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSC2007 touchscreen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458378#M71730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a imx6 dts that uses tsc2007:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/arch/arm/boot/dts/imx6qdl-tx6.dtsi?id=refs/tags/v4.4-rc3#n282" title="https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/arch/arm/boot/dts/imx6qdl-tx6.dtsi?id=refs/tags/v4.4-rc3#n282"&gt;https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/arch/arm/boot/dts/imx6qdl-tx6.dtsi?id=refs/tags/v4.…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you configured GPIO3_21 as GPIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, does it help if you do "interrupts = &amp;lt;21 0&amp;gt;;" instead?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 21:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458378#M71730</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-12-03T21:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using TSC2007 touchscreen</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458379#M71731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;What the "126" at "clocks = &amp;lt;&amp;amp;clks 126&amp;gt;;" means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is IMX6QDL_CLK_I2C2 defined in&amp;nbsp; .../include/dt-bindings/clock/imx6qdl-clock.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 02:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-TSC2007-touchscreen/m-p/458379#M71731</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-04T02:02:02Z</dc:date>
    </item>
  </channel>
</rss>