<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question, i.MX6Q DVI_mode setting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458327#M71725</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hello,&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&amp;gt; &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Should the customer set the bit to 0(DVI mode)?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Also, when using HDMI-&amp;gt;DVI adapter, the following from Artur may be helphul :&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; "Finally, I've been able to make the 1280x1024 DVI monitor (LG Flatron 1710) work &lt;/P&gt;&lt;P&gt;with the i.MX6Q SDP board running L3.10.53 BSP through the HDMI output and &lt;/P&gt;&lt;P&gt;passive HDMI-&amp;gt;DVI adapter. To do it, I've added the new 'allow_noncea=1' &lt;/P&gt;&lt;P&gt;environment variable in the U-Boot configuration and the following arguments to &lt;/P&gt;&lt;P&gt;the kernel command line: 'video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'. The &lt;/P&gt;&lt;P&gt;setup looked like following for my case of booting from external SD card on the &lt;/P&gt;&lt;P&gt;SD3 (J507 connector on the board) interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;setenv allow_noncea 1&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These settings forcedly fix the HDMI resolution to 1280x1024 and make the DVI monitor work correctly."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Aug 2015 04:05:52 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-08-31T04:05:52Z</dc:date>
    <item>
      <title>Question, i.MX6Q DVI_mode setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458323#M71721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the setting of the DVI_mode bitfield in i.MX6Q HDMI_FC_INVIDCONF register.&lt;/P&gt;&lt;P&gt;Could you show me the exact difference in terms of i.MX6 behavior between setting the DVI_mode bit and clearing the bit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 02:48:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458323#M71721</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-08-24T02:48:43Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q DVI_mode setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458324#M71722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; According to HDMI specs, all HDMI Sources shall be compatible with DVI compliant &lt;BR /&gt;sink devices (i.e. “monitors” or “displays”) through the use of a passive cable converter. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;The DVI_mode bit is used to meet&amp;nbsp; the requirement for DVI Compatibility.&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2015 06:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458324#M71722</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-27T06:40:22Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q DVI_mode setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458325#M71723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miyamoto,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're currently trying to get our iMX6-based product to output video to DVI screens. So far we've found that HDMI monitors, and monitors with dual HDMI/DVI ports work fine, but DVI-only monitors (especially older models) will only display video if I manually set this bit to 0 (DVI mode). It seems to default to 1 (HDMI mode) at least once the kernel and video driver is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem I have found is that even with this bit set to 0, DVI-only monitors do not maintain sync very well, and I have yet to find a way of setting it without JTAG.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2015 10:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458325#M71723</guid>
      <dc:creator>danielleloader</dc:creator>
      <dc:date>2015-08-27T10:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q DVI_mode setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458326#M71724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your information.&lt;/P&gt;&lt;P&gt;I am still not sure what is actually changed by setting or clearing the bit.&lt;/P&gt;&lt;P&gt;My customer will use the port as DVI not HDMI.&lt;/P&gt;&lt;P&gt;Should the customer set the bit to 0(DVI mode)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2015 14:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458326#M71724</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-08-28T14:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q DVI_mode setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458327#M71725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hello,&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;&amp;gt; &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Should the customer set the bit to 0(DVI mode)?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Also, when using HDMI-&amp;gt;DVI adapter, the following from Artur may be helphul :&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; "Finally, I've been able to make the 1280x1024 DVI monitor (LG Flatron 1710) work &lt;/P&gt;&lt;P&gt;with the i.MX6Q SDP board running L3.10.53 BSP through the HDMI output and &lt;/P&gt;&lt;P&gt;passive HDMI-&amp;gt;DVI adapter. To do it, I've added the new 'allow_noncea=1' &lt;/P&gt;&lt;P&gt;environment variable in the U-Boot configuration and the following arguments to &lt;/P&gt;&lt;P&gt;the kernel command line: 'video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'. The &lt;/P&gt;&lt;P&gt;setup looked like following for my case of booting from external SD card on the &lt;/P&gt;&lt;P&gt;SD3 (J507 connector on the board) interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;setenv allow_noncea 1&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'&lt;/P&gt;&lt;P&gt;U-Boot&amp;gt;saveenv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These settings forcedly fix the HDMI resolution to 1280x1024 and make the DVI monitor work correctly."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 04:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-DVI-mode-setting/m-p/458327#M71725</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-31T04:05:52Z</dc:date>
    </item>
  </channel>
</rss>