<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mfw_isink with queue issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfw-isink-with-queue-issue/m-p/457992#M71666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls try to add "device=/dev/vedio17" end of the command, and the performance of isink is worse than v4lsink, if you just output one video, pls use v4lsink.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 08:08:21 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2015-09-23T08:08:21Z</dc:date>
    <item>
      <title>mfw_isink with queue issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfw-isink-with-queue-issue/m-p/457991#M71665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use mfw_isink in a pipeline requiring a queue. The pipeline "gst-launch tvsrc ! queue ! mfw_v4lsink"&amp;nbsp; works OK, but when I replace mfw_v4lsink with mfw_isink, it crashes with the following messages:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MFW_GST_tvsrc_PLUGIN 3.0.11 build on May 29 2015 17:43:14.&lt;/P&gt;&lt;P&gt;set color key&lt;/P&gt;&lt;P&gt;MFW_GST_ISINK_PLUGIN 3.0.11 build on May 29 2015 17:43:31.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;should set the input to 1&lt;/P&gt;&lt;P&gt;Pipeline is live and does not need PREROLL ...&lt;/P&gt;&lt;P&gt;Setting pipeline to PLAYING ...&lt;/P&gt;&lt;P&gt;New clock: GstSystemClock&lt;/P&gt;&lt;P&gt;ERROR: from element /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0: Internal data flow error.&lt;/P&gt;&lt;P&gt;Additional debug info:&lt;/P&gt;&lt;P&gt;/opt/oe-toradex/build/out-glibc/work/armv7at2hf-vfp-neon-angstrom-linux-gnueabi/gstreamer/0.10.36-r2/gstreamer-0.10.36/libs/gst/base/gstbasesrc.c(2625): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0:&lt;/P&gt;&lt;P&gt;streaming task paused, reason error (-5)&lt;/P&gt;&lt;P&gt;Execution ended after 1217918877 ns.&lt;/P&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;/P&gt;&lt;P&gt;Setting pipeline to READY ...&lt;/P&gt;&lt;P&gt;can not create threadmfw_gst_isink_setcaps:1489&lt;/P&gt;&lt;P&gt;Setting pipeline to NULL ...&lt;/P&gt;&lt;P&gt;Freeing pipeline ...&lt;/P&gt;&lt;P&gt;[---&amp;gt;FINALIZE isink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know how to fix that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 04:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfw-isink-with-queue-issue/m-p/457991#M71665</guid>
      <dc:creator>alexanderkhudos</dc:creator>
      <dc:date>2015-09-18T04:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: mfw_isink with queue issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfw-isink-with-queue-issue/m-p/457992#M71666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls try to add "device=/dev/vedio17" end of the command, and the performance of isink is worse than v4lsink, if you just output one video, pls use v4lsink.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 08:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfw-isink-with-queue-issue/m-p/457992#M71666</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2015-09-23T08:08:21Z</dc:date>
    </item>
  </channel>
</rss>